Building and debugging in LS1028ARDB (vs T1040D4-RDB)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Building and debugging in LS1028ARDB (vs T1040D4-RDB)

跳至解决方案
126 次查看
ricardofranca
Contributor III

Hello,

I have had some experience with MPC and QorIQ PowerPC-based MCUs/processors and I intend to give a try to the newer ARM-based families.

When working with QorIQ devices, I used to do some basic testing either by calling my applications directly from U-boot (uploading it via serial or Ethernet having built it with the GHS compiler) or by running it from the GHS debugging envionment, uploading it and debugging it with the GHS probe.

Are these two scenarios available in the LS1028A evaluation board? I.e., can I 1) run some bare-metal application by simply using the "go" U-boot command; 2) Use the GHS environment for more detailed debugging?

Thanks,

Ricardo

标签 (1)
0 项奖励
回复
1 解答
105 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

1) Yes you can run baremetal code

2) you have to go with Greenhills for detail on it, it's supported.

 

Regards

在原帖中查看解决方案

1 回复
106 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

1) Yes you can run baremetal code

2) you have to go with Greenhills for detail on it, it's supported.

 

Regards