I'm trying to write a bare-metal program that accesses the QSPI on my LS1021A-TWR X3 board. Neither my program, nor the CodeWarrior flash programmer task can access it. The Flash Programmer actually reports success of the diagnoses, but the ID it reports tells another story:
Flash Information
=================
Flash Manufacturer ID :0x000000FF
Flash Device ID (byte1) :0x000000FF
Flash Device ID (byte2) :0x000000FF
Flash Device ID (byte3) :0x0000FFFF
Secure Device Verification:0x00000000
Diagnose Succeeded
I'm debugging with Code Warrior TAP over USB.
Do I need a special configuration of Switches or config files in order to access the flash? My project is using the init file provided by CodeWarrior LS1021A-TWR_Init.tcl. Thanks.
已解决! 转到解答。
Make sure you use the correct setting for Target RAM:
And also correct Address Offset when programming into qspi:
fl::target -lc "ls1021atwr-core0_RAM_LS1021ATWR_Download"
fl::target -b 0x10000000 0x20000
fl::target -v off -l off
cmdwin::fl::device -d "N25Q128A" -o "16Mx8x1" -a 0x40000000 0x40ffffff
cmdwin::fl::image -f "X:\\QorIQ-SDK-V1.9-20151210-yocto\\build_ls1021atwr\\tmp\\deploy\\images\\ls1021atwr\\u-boot-qspi.bin" -t "Auto Detect" -re off -oe on -o 0x40000000
cmdwin::fl::write
Beginning Operation ...
-------------------------
Programming file X:\QorIQ-SDK-V1.9-20151210-yocto\build_ls1021atwr\tmp\deploy\images\ls1021atwr\u-boot-qspi.bin
Auto-detection is successful.
File is of type Binary/Raw Format.
Performing target initialization ...
Downloading Flash Device Driver ...
Reading flash ID ...
Auto-detection is successful.
File is of type Binary/Raw Format.
Downloading 0x00010000 bytes to be programmed at 0x40000000
Executing program ....
Program Command Succeeded
Downloading 0x00010000 bytes to be programmed at 0x40010000
Executing program ....
Program Command Succeeded
Downloading 0x00010000 bytes to be programmed at 0x40020000
Executing program ....
Program Command Succeeded
Downloading 0x00010000 bytes to be programmed at 0x40030000
Executing program ....
Program Command Succeeded
Downloading 0x00010000 bytes to be programmed at 0x40040000
Executing program ....
Program Command Succeeded
Downloading 0x00010000 bytes to be programmed at 0x40050000
Downloading 0x0000AA60 bytes to be programmed at 0x40060000
Executing program ....
Program Command Succeeded
cmdwin::fl::dump -range 0x40000000 0x40080000 -t "Binary/Raw Format" -o "C:\\Users\\b11883\\Desktop\\qspi_dump.bin"
-------------------------
Downloading Flash Diagnostics Driver ...
Reading flash ID ...
Dumping flash region: 0x40000000 - 0x40080000 to C:\Users\b11883\Desktop\qspi_dump.bin
Running Dump Flash ...
Running Dump Flash ...
Running Dump Flash ...
Running Dump Flash ...
Running Dump Flash ...
Dump Flash Succeeded
Adrian
To summarize - the things that helped me:
* Configure the run configuration with the QSPI cfg file. For me, this was at: C:\Freescale\CW4NET_v2016.01\CW_ARMv7\ARMv7\ARM_Support\Configuration_Files\jtag_chains\LS102xATWR_RCW_1000-300-1600_QSPI.txt
* I changed a value in that file as described in this thread (search for "4108"). I haven't checked to see if it works without that change.
* SW2: 0010_0111
* Setting the proper offsets in the flash programmer task
* 0x10000000 for the Target RAM
* 0x40000000 for the "Apply Address Offset" option
* 0x40000000 for the Flash Device Base Address (column in table in "Add Program/Verify Action" dialog)
* booting from SDCard with the .bin attached in this thread
Make sure you use the correct setting for Target RAM:
And also correct Address Offset when programming into qspi:
fl::target -lc "ls1021atwr-core0_RAM_LS1021ATWR_Download"
fl::target -b 0x10000000 0x20000
fl::target -v off -l off
cmdwin::fl::device -d "N25Q128A" -o "16Mx8x1" -a 0x40000000 0x40ffffff
cmdwin::fl::image -f "X:\\QorIQ-SDK-V1.9-20151210-yocto\\build_ls1021atwr\\tmp\\deploy\\images\\ls1021atwr\\u-boot-qspi.bin" -t "Auto Detect" -re off -oe on -o 0x40000000
cmdwin::fl::write
Beginning Operation ...
-------------------------
Programming file X:\QorIQ-SDK-V1.9-20151210-yocto\build_ls1021atwr\tmp\deploy\images\ls1021atwr\u-boot-qspi.bin
Auto-detection is successful.
File is of type Binary/Raw Format.
Performing target initialization ...
Downloading Flash Device Driver ...
Reading flash ID ...
Auto-detection is successful.
File is of type Binary/Raw Format.
Downloading 0x00010000 bytes to be programmed at 0x40000000
Executing program ....
Program Command Succeeded
Downloading 0x00010000 bytes to be programmed at 0x40010000
Executing program ....
Program Command Succeeded
Downloading 0x00010000 bytes to be programmed at 0x40020000
Executing program ....
Program Command Succeeded
Downloading 0x00010000 bytes to be programmed at 0x40030000
Executing program ....
Program Command Succeeded
Downloading 0x00010000 bytes to be programmed at 0x40040000
Executing program ....
Program Command Succeeded
Downloading 0x00010000 bytes to be programmed at 0x40050000
Downloading 0x0000AA60 bytes to be programmed at 0x40060000
Executing program ....
Program Command Succeeded
cmdwin::fl::dump -range 0x40000000 0x40080000 -t "Binary/Raw Format" -o "C:\\Users\\b11883\\Desktop\\qspi_dump.bin"
-------------------------
Downloading Flash Diagnostics Driver ...
Reading flash ID ...
Dumping flash region: 0x40000000 - 0x40080000 to C:\Users\b11883\Desktop\qspi_dump.bin
Running Dump Flash ...
Running Dump Flash ...
Running Dump Flash ...
Running Dump Flash ...
Running Dump Flash ...
Dump Flash Succeeded
Adrian
Please use attached uboot for sd-card, which enable qspi (this is also available in SDK 1.9). To program this uboot into the sd card you can use CW, import LS102xATWR_SD_FLASH Target Tasks, and set the offset address to 0x1000. Or you can mount your sd card into a host linux and use the command:
sudo dd if=u-boot-sdcard-qspi.bin of=/dev/<sd card mount> seek=8
Adrian
Interaction with flash via CW and TAP is still the same. "Operation unsupported". There is some good news - booting from the SDCard with the image you attached to your last post worked. I was able to sf probe, then read flash. And, the data I read from U-boot is the same as the data I read from CW at addr 0x40000000. So some parts of it are working. I'm just not able to program flash with CW and TAP. Attached is a screenshot immediately after attempting a flash programming task:
The diagnose operation and my application still read all 0xFF as well.
I will attempt a program and erase from u-boot just to verify that works.
I suspect there's something wrong with my debug configuration. Is it possible that there's a step-by-step procedure documented for programming QSPI flash? Maybe I can take my projects and debug configurations out of the equation...
Here is my Diagnose running on board booting from sd, using u-boot-sdcard-qspi.bin and SW2: 0010_0111
fl::target -lc "ls1021atwr-core0_RAM_LS1021ATWR_Download"
fl::target -b 0x10000000 0x20000
fl::target -v off -l off
cmdwin::fl::device -d "N25Q128A" -o "16Mx8x1" -a 0x40000000 0x40ffffff
cmdwin::fl::diagnose full
Beginning Operation ...
-------------------------
Performing target initialization ...
Downloading Flash Diagnostics Driver ...
Reading flash ID ...
Running Diagnostics ...
Running Diagnostics ......................................
Sector Map (read from target)
=============================
Sector 00000: 0x40000000 - 0x4000FFFF Size=0x00010000 unprotected programmed
Sector 00001: 0x40010000 - 0x4001FFFF Size=0x00010000 unprotected programmed
Sector 00002: 0x40020000 - 0x4002FFFF Size=0x00010000 unprotected programmed
Sector 00003: 0x40030000 - 0x4003FFFF Size=0x00010000 unprotected programmed
Sector 00004: 0x40040000 - 0x4004FFFF Size=0x00010000 unprotected programmed
Sector 00005: 0x40050000 - 0x4005FFFF Size=0x00010000 unprotected programmed
Sector 00006: 0x40060000 - 0x4006FFFF Size=0x00010000 unprotected programmed
Sector 00007: 0x40070000 - 0x4007FFFF Size=0x00010000 unprotected blank
.....
Flash Information
=================
Flash Manufacturer ID :0x00000020
Flash Device ID (byte1) :0x000000BA
Flash Device ID (byte2) :0x00000018
Flash Device ID (byte3) :0x00004323
Secure Device Verification:0x00000000
Diagnose Succeeded
Adrian
Still no luck when booting from the SD card. I tried to use the SDCard that came with the dev board. I don't know think this was the proper image because, even though it booted to U-Boot, there was no sf command in U-boot, just nor flash commandss. Unless you have more suggestions, I'll delay debugging this issue until the custom HW arrives. Thanks for the help.
Hi Janson,
To be able to access qspi, with no switch settings, you have to use RCW12 = 0x20024800. So, you can use jtag chain file as Target type in CW and add the new value for RCW12 in rcw index 4108.
Also, please try a Program/Verify Action, follow by a Dump Action. It is possible that Flash Programmer to return wrong Manufacturer ID.
Adrian
This first response got lost, so I'll post again...
I added the file C:\Freescale\CW4NET_v2016.01\CW_ARMv7\ARMv7\ARM_Support\Configuration_Files\jtag_chains\LS102xATWR_RCW_1000-300-1600_QSPI.txt
to my debug config target type. In that file, I changed (4108 0x20024000) to (4108 0x20024800).
Is this the filetype to use, or were you referring to the jtag.cfg type file?
My app and Flash Programmer still not working, but as posted previously, I now read 0xFF from 0x40000000 instead of 0x00.
My config:
I wonder if maybe I don't have the clocks configured properly. The QSPI module is apparently sampling the inputs, because it's placing the correct number of 0xFF bytes in the RX buffer. Is that a good indication that the QSPI clock is running?
I'm not doing any explicit configuration of the clocks - just using what's on the dev board and is configured in the QSPI debug config file...
Programmer task still returns 0xFF after setting SW2.5 = 0.
Sector 00255: 0x00FF0000 - 0x00FFFFFF Size=0x00010000 unprotected programmed
Flash Information
=================
Flash Manufacturer ID :0x000000FF
Flash Device ID (byte1) :0x000000FF
Flash Device ID (byte2) :0x000000FF
Flash Device ID (byte3) :0x0000FFFF
Secure Device Verification:0x00000000
It does seemed to have changed the readout - from 0x40000000 I now read 256 bytes of 0x55, 256 bytes of 0xAA, then all 0xFF.
I removed the "erase before programming option" in the flash programmer task, but same problem:
fl::target -lc "QSPIFlashTest-core0_RAM_LS1021ATWR_Download"
fl::target -b 0x80000000 0x4000000
fl::target -v off -l off
cmdwin::fl::device -d "N25Q128A" -o "16Mx8x1" -a 0x0 0xffffff
cmdwin::fl::image -f "C:\\Freescale\\CW4NET_v2016.01\\CW_ARMv7\\ARMv7\\ARM_Support\\FlashToolKit\\TestSrecFiles\\8k_at_0.S" -t "Auto Detect" -re off -oe off
cmdwin::fl::write
Beginning Operation ...
-------------------------
Programming file C:\Freescale\CW4NET_v2016.01\CW_ARMv7\ARMv7\ARM_Support\FlashToolKit\TestSrecFiles\8k_at_0.S
Auto-detection is successful.
File is of type Motorola S-Record Format.
Performing target initialization ...
Downloading Flash Device Driver ...
Reading flash ID ...
Auto-detection is successful.
File is of type Motorola S-Record Format.
Downloading 0x00002000 bytes to be programmed at 0x00000000
Executing program ....
Error: Program failed. Flash driver reports the following error(s): Operation Unsupported
Error: Program failed. Flash driver reports the following error(s): Operation Unsupported