Accessible leds GPIO pin numbers on LS1046ARDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Accessible leds GPIO pin numbers on LS1046ARDB

598 Views
itzik_sherf
Contributor I

Hello

Trying to control the accessible LEDs on LS1046ARDB via Linux userspace following this information:

 https://www.kernel.org/doc/Documentation/gpio/sysfs.txt 

I know that NXP SDK supports SYSFS possibility GPIO using  from userspace, and I've configured the kernel with COFIG_GPIO_SYSFS.

The issue is, that in order to actually control LEDs/GPIO, I need to know the pin numbers of the board GPIOs.

I did not manage to find any information about the board schematic or even GPIO pinout list.

Can someone help please?

0 Kudos
1 Reply

562 Views
ufedor
NXP Employee
NXP Employee

By default (RCW from the NXP LSDK) there are no GPIO signals configured on the LS1046ARDB - refer to the U-Boot log and the QorIQ LS1046A Reference Manual, 3.4 Signal multiplexing details.

0 Kudos