How to customize LITB image from LSDK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to customize LITB image from LSDK

How to customize LITB image from LSDK

This topic shows steps to customize LITB by using a different kernel image instead of the existing kernel image.

  1. Browse to the FlexBuild installation directory.
  2. Modify the kernel image in linux_arm64_LS.its.
    $ vi configs/linux/linux_arm64_LS.its

    linux_arm64_LS.png

  3. Save the changes done in the file.
  4. Generate LITB using flex-builder.
    $ source setup.env
    $ flex-builder -i mkitb -r <distro_type>:<distro_scale> -a <arch>

    For example:

    $ source setup.env
    $ flex-builder -i mkitb -r ubuntu:main -a arm64
    
    INSTRUCTION: mkitb
    DISTRO TYPE: ubuntu
    DISTRO SCALE: main
    ....
    ....
    /home/flexbuild_lsdk2004/build/images/lsdk2004_ubuntu_main_LS_arm64.itb     [Done]

     

    Note: To create .itb file directly from .its file, run this command: mkimage -f <xyz.its> <xyz.itb>

  5. Connect to the board console via terminal and run following commands at U-boot to boot the board with customized LITB.
    => ping $serverip
    Using e1000#0 device
    host 192.168.3.1 is alive
    =>
    Using e1000#0 device
    host 192.168.3.1 is alive
    => tftp 0xa0000000 lsdk2004_ubuntu_main_LS_arm64.itb
    Using e1000#0 device
    TFTP from server 192.168.3.1; our IP address is 192.168.3.49
    Filename 'lsdk2004_ubuntu_main_LS_arm64.itb'.
    Load address: 0xa0000000
    Loading: #################################################################
             #################################################################
             #################################################################
             #################################################################
             #################################################################
             #################################################################
             ####################################
             9.8 MiB/s
    done
    Bytes transferred = 683506200 (28bd7a18 hex)
    => bootm 0xa0000000#lx2160ardb
    ## Loading kernel from FIT Image at a0000000 ...
       Using 'lx2160ardb' configuration
       Trying 'kernel' kernel subimage
         Description:  ARM64 Kernel
         Created:      2021-02-03   6:01:29 UTC
         Type:         Kernel Image
         Compression:  gzip compressed
         Data Start:   0xa00000d0
         Data Size:    14086432 Bytes = 13.4 MiB
    

     

  6. Check timestamp in boot log to ensure that the board is booted with the updated kernel image in the customized LITB.

     

    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd083]
    [    0.000000] Linux version 5.4.3 (test@Ubuntu-18) (gcc version 7.5.0 (Ubuntu/Linaro 7.5.0-3ubuntu1~18.04)) #1 SMP PREEMPT Wed Feb 3 00:04:09 IST 2021
    [    0.000000] Machine model: NXP Layerscape LX2160ARDB
    [    0.000000] earlycon: pl11 at MMIO32 0x00000000021c0000 (options '')
    [    0.000000] printk: bootconsole [pl11] enabled
    [    0.000000] efi: Getting EFI parameters from FDT:
    

     

无评分
版本历史
最后更新:
‎02-17-2021 03:04 AM
更新人: