Content originally posted in LPCWare by rouxfederico on Tue Nov 25 12:17:37 MST 2014
I'been using LPCXpresso from the version#3 to the lastest version. I see the following problems with the IDE with LPC1769 or LPC1115:
> When you use more than 3 breakpoints or watchpoints, the debug session crashes or it doesn't start, even if the breakpoints are not enabled.
> Sometimes the IDE let you put some breakpoints but the program doesn't stop in that point.
> The driver of the LPCXpresso crashes and you have to reset the board.
> When you are debbugging a program, the "step over" button sometimes jump to an unexpected position of the program, and then goes on.
There are more things, but these are the ones I remember now.