Content originally posted in LPCWare by CodeRedSupport on Wed Aug 11 06:31:52 MST 2010
Before starting a debug session, the debug driver is run to look for possible debug targets (LPC-Link, Red Probe, etc). If a single debug target is found, then it will use that; if multiple targets are found, the user is prompted to select one.
From your description, my guess is that the debug driver is crashing when looking for for a debug target.
To help us determine the error, can you try running the following commands from the command line and post the output to this thread:
<install>/bin/crt_emu_lpc11_13_nxp -info-emu
<install>/bin/crt_emu_lpc11_13_nxp -info-emu -wire=hid
<install>/bin/crt_emu_lpc11_13_nxp -info-emu -wire=winusb
Thanks