connect to emulator or board error LPC1114 Xpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

connect to emulator or board error LPC1114 Xpresso

692 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by GreenITguy on Fri Apr 22 22:12:02 MST 2011
I am getting a 'No emulator or board available' while trying to debug in Windows 7 64bit.

I have done the following things in vain and now at my wits end... please help !!

1. Tried another board
2. Verified LPC11xx is selected MCU
3. Removed the USB DFU device and reinstalled with the drivers included in the LPCXpresso setup
4. Manually reset the MCU to ISP mode

I see others have also faced the problem but it is difficult to figure out what is the fix
0 Kudos
7 Replies

663 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by travisf on Mon Oct 29 05:44:19 MST 2012
I was able to get this working by running LPCXpresso as an administrator on Windows 7 64bit.
0 Kudos

663 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by GreenITguy on Sat Apr 23 16:32:30 MST 2011
I managed to investigate and resolve the issue myself. I am documenting it here so that others can benefit.

I looked up the build log files in <workspace folder>\.metadata\.log and noticed the following error:
[B]java.lang.Exception: Input Error: There is no script engine for file extension ".vbs".
[/B]
I changed the file association for .vbs to WScript but the error did not go away.

A quick google-ing turned up this 3 step process
http://www.nilpo.com/2009/07/windows-xp/error-there-is-no-script-engine-for-file-extension/

Just follow the 3 steps and restart.

Voila ! the thing works now !
0 Kudos

663 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by GreenITguy on Sat Apr 23 07:25:04 MST 2011
Hello Code Red Support,

Here is the diagnostic information:


D:\nxp\lpcxpresso_3.6.3_317\bin>cd Scripts

D:\nxp\lpcxpresso_3.6.3_317\bin\Scripts>bootLPCXpresso winusb
Booting LPC-Link with LPCXpressoWIN.enc
Press any key to continue . . .
D:\nxp\lpcxpresso_3.6.3_317\bin\Scripts>set CRT_DEBUG_TRACE=1

D:\nxp\lpcxpresso_3.6.3_317\bin\Scripts>cd ..

D:\nxp\lpcxpresso_3.6.3_317\bin>crt_emu_lpc11_13_nxp -info-emu -wire=winusb
Ni: LPCXpresso Debug Driver v2.0 (Mar 29 2011 00:09:34)
1 Emulators available:
0. T1S6RGRIA    LPC-Link Probe v1.1 (Code Red - LPCXpresso)

D:\nxp\lpcxpresso_3.6.3_317\bin>crt_emu_lpc11_13_nxp -info-target -pLPC1114/302
-wire=winusb -4
Ni: LPCXpresso Debug Driver v2.0 (Mar 29 2011 00:09:34)
Nc: Looked for chip XML file in D:/nxp/lpcxpresso_3.6.3_317/bin/LPC1114/302.xml

Nc: Looked for vendor directory XML file in D:/nxp/lpcxpresso_3.6.3_317/bin/nxp_
directory.xml

Nc: Found generic directory XML file in D:/nxp/lpcxpresso_3.6.3_317/bin/crt_dire
ctory.xml

AP Ack: 04
Nc: Mem-AP ID: 0x04770021  ROM Addr: 0xE00FF003
Nc: Emu(0): Conn&Reset. DpID:  BB11477. Info: T1S6RGRIA
Nc: SWD Frequency: 3000 KHz. RTCK: False. Vector catch: False.
Nc: Packet delay: 0  Poll delay: 0.
Nc: NXP: LPC1114/302  Part ID: 0x2540102B


----
[B][COLOR=Navy]At this point it crashes and returns me to the command prompt[/COLOR][/B]

Here is the crash message:


Problem signature:
  Problem Event Name:APPCRASH
  Application Name:crt_emu_lpc11_13_nxp.exe
  Application Version:0.0.0.0
  Application Timestamp:4d9185b2
  Fault Module Name:crt_emu_lpc11_13_nxp.exe
  Fault Module Version:0.0.0.0
  Fault Module Timestamp:4d9185b2
  Exception Code:c0000005
  Exception Offset:0000faed
  OS Version:6.1.7601.2.1.0.256.1
  Locale ID:1033
  Additional Information 1:0a9e
  Additional Information 2:0a9e372d3b4ad19135b953a78882e789
  Additional Information 3:0a9e
  Additional Information 4:0a9e372d3b4ad19135b953a78882e789
0 Kudos

663 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Sat Apr 23 01:17:44 MST 2011
Please run the diagnostics suggest by larryvc and post your results.
0 Kudos

663 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larryvc on Fri Apr 22 23:28:32 MST 2011
You did broke your board?:D

I was hoping that one of those would have been a possibility.

Can you post the exact error message you are receiving.

Also try running the following diagnostics.  Follow them to the letter and post the full results of each command back here.

http://support.code-red-tech.com/CodeRedWiki/LPCLinkDiagnostics

CodeRedSupport will probably pick up from here later.
0 Kudos

663 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by GreenITguy on Fri Apr 22 22:53:51 MST 2011
Larry,

I appreciate your quick response! and here are my anwsers:


s Win7 running native i.e not on a virtual machine?
Native Win7

Is your USB port powered i.e. not on an unpowered USB hub?
USB port powered

Is your LPCXpresso1114 standalone or are you using it with an EA base board? If on a base board, the base board needs it's own power.
Standalone

When you installed LPCXpresso were you an Administrator?
Yes

Have you tried a different USB cable?
Yes
0 Kudos

663 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by larryvc on Fri Apr 22 22:33:55 MST 2011
Hi GreenITguy,

Welcome to the forum.

Quite a few people, including myself, have installed and are running LPCXpresso on Win 7 64-bit without any problems.  You should not have had to uninstall the DFU drivers to get up and running.

Just a few questions to get the pump primed for everyone.:)

Is Win7 running native i.e not on a virtual machine?

Is your USB port powered i.e. not on an unpowered USB hub?

Is your LPCXpresso1114 standalone or are you using it with an EA base board?  If on a base board,  the base board needs it's own power.

When you installed LPCXpresso were you an Administrator?

Have you tried a different USB cable?

That should be enough for now.  I really need to write a script for this.:)

Answering these will help all of us understand what you are working with.  We're all in different timezones and we come and go frequently.

Larry
0 Kudos