Using an LPV14111 debugging under LPCxpresso. Could set breakpoints then suddenly all break points appear with a diagonal line through them and nothing happens when they are hit (i.e. cannot stop and debug program). I do build the debug version and can see the DEBUG env variable in the build lines. What have I miss set in the LPCxpresso.
Also under OSX 10.13.3 is crashes randomly (just disappears and have to re-start.)
Thanks for the help.
已解决! 转到解答。
Just tried to reset the machine LPCXpresso runs on and that made no difference. Program is built Debug and loads and runs just fine but breakpoints still show diagonal line through them not just a blue dot. And program does not stop.