The CAN RTX application does not run after a power restart.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The CAN RTX application does not run after a power restart.

158 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by pavan_munavalli on Thu Jan 29 07:59:48 MST 2015
Hello all,

I am stuck in a weird problem.

I am programming a CAN application. The stand alone CAN program (which is based on the example program in the LPCopen) works perfectly fine, even after a power restart.

Now I have included the same CAN application into the RTX(based on CMSIS rtos). The application works fine, but does not work after a power restart. Also, the CAN with RTX runs only after running the CAN standalone application which works pretty well.

I have just included the CAN standalone application into a single thread and nothing more.

Can you guys give me an idea where I might have the problem ?

Thanks,
Pavan.
0 Kudos
0 Replies