SVN integration in LPCXpresso

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SVN integration in LPCXpresso

372 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kralux on Wed Nov 17 15:07:31 MST 2010
Is there anyway to have SVN handled from within the LPCXpresso IDE?

Good IDEs like IntelliJ IDEA do integrate most common source control versioning protocols like CVS, SVN, ...

Thank you.

Original Attachment has been moved to: 1100840_LPC1778-PLL-Calculator.zip

0 项奖励
2 回复数

245 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by kralux on Thu Nov 18 11:35:08 MST 2010
:) That is great!
Thanks a lot.
0 项奖励

245 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by CodeRedSupport on Thu Nov 18 00:56:18 MST 2010
LPCXPresso is based on Eclipse, for which there are (literally) hundreds of enhancements (plugins) available, including two for integration with Subversion. Details on integration with some version control systems can be found on our support system, here:
http://support.code-red-tech.com/CodeRedWiki/VersionControl

If it helps, internally, we use Subclipse.
0 项奖励