Peripherals window shows just base addresses, not single entries

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Peripherals window shows just base addresses, not single entries

179 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by StephenHawkings on Sun Mar 13 05:53:31 MST 2011
Dear Collegues,
I wonder how I can change the "Peripherals" window in that way, that I can see the single entries, for example LPC_IOCON->PIO1_7. Still I see the base address only, and I can't find a solution to expand the peripherals (like folders or so.) Can anybody help me?`
Thanks a lot!!
0 项奖励
2 回复数

169 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by StephenHawkings on Sun Mar 13 07:04:29 MST 2011
It didn't; so I closed XPRESSO and re-opened again.
Now it works, and I can tick the boxes at the left side of the peripherals, and I can see them also then in the memory window.
Really strange behaviour, I think.
But now, it works :) .
0 项奖励

169 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sun Mar 13 06:51:45 MST 2011
1. Select GPIO1 in 'Peripherals' view

2. Expand GPIO1 in 'Memory' view

Isn't that working?
0 项奖励