Mbed 1768 - LPCXpresso IDE SWV output not available

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Mbed 1768 - LPCXpresso IDE SWV output not available

310 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ScubaBoy on Mon Nov 09 01:32:43 MST 2015
Hi,

I've taken the simple LED blinking code example and exported to LPCXpresso builds and deploys ok and I'm able to step through the code using the debugger. However I'm trying to enable the SWV feed but for some reason LPCXpresso does not detect any SWV capability:

HasSWV = FALSE HasETM = FALSE HasJTAG = FALSE HasSWD = TRUE Probe Type = CMSIS-DAP

Is this feature not supported by the mbed firmware?

Thanks
0 项奖励
4 回复数

299 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Mon Nov 09 05:57:58 MST 2015
I'm not sure if you can connect an external debug probe to the mbed board. If you can, then yes, you will have access to SWV.

Suggest you read the FAQ...
https://www.lpcware.com/content/faq/lpcxpresso/trace-overview
0 项奖励

299 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ScubaBoy on Mon Nov 09 05:32:40 MST 2015
would I have access to the SWV output if I used the following debug board:

LPC-Link 2

0 项奖励

299 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ScubaBoy on Mon Nov 09 02:13:09 MST 2015
Thanks for the quick response.
0 项奖励

299 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by vtw.433e on Mon Nov 09 02:00:26 MST 2015
SWV is not supported by CMSIS-DAP...
0 项奖励