Lpc1224 deep sleep mode wakeup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Lpc1224 deep sleep mode wakeup

181 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by IanJames on Tue Jul 09 05:26:55 MST 2013
Hi,

I am trying to put an LPC1224 in to Deep Sleep mode and wake it with a falling edge on LPC_GPIO0_10. The input has an external 10k pull up on it and I know it works because I output LPC_GPIO->PIN to a UART when processor is awake.

The problem is not going to sleep but waking up.

Grounding LPC_GPIO0_10 does not wake it up - only a power cycle does.

Anyone know what I am doing wrong?

Thanks,

Ian


void GotoSleep(void)
{
        LPC_IOCON->PIO0_10 &= ~0x07; 

//Choose Deep sleep mode
SCB->SCR |= ((1 << 2));

LPC_SYSCON->PDSLEEPCFG = 0x0000FFFF;
LPC_SYSCON->PDRUNCFG &= (~(0xFF));
LPC_SYSCON->INTNMI = 0x00000010;// PIO0_10 SCL

// Set up the Power Management Unit
LPC_PMU->PCON &= ~(1 << 1); //DPDEN = 0

//Set up the wake up
LPC_SYSCON->STARTAPRP0    &= ~(1 << 10);// Falling edge
LPC_SYSCON->STARTRSRP0CLR |=  (1 << 10);
LPC_SYSCON->STARTERP0     |=  (1 << 10);

NVIC_EnableIRQ(WAKEUP10_IRQn);

LPC_SYSCON->PDAWAKECFG = ~(0x01 < 1) | ~(0x01 << 7);

LPC_SYSCON->MAINCLKSEL = 0x00; // IRC
LPC_SYSCON->MAINCLKUEN = 0x00; // effect the change
LPC_SYSCON->MAINCLKUEN = 0x01;

/* And so to sleep zzzzzzzzzzzz */
__WFI();
}




void WAKEUP_IRQHandler(void)
{
;
}
0 Kudos
Reply
0 Replies