Content originally posted in LPCWare by Roland on Tue Aug 09 07:49:05 MST 2011
I did
C:\nxp\LPCXpresso_4.0.6_152\lpcxpresso>
C:\nxp\LPCXpresso_4.0.6_152\lpcxpresso>Path=C:\WINDOWS\system32;C:\WINDOWS;C:\WINDOWS\System32\Wbem;
lpcxpresso came up, I got a warning from WINDOWS that network access is blocked for program lpcxpresso. Then I pushed the debug-button, the program was loaded and is still executing. In this situation I prepared path0.txt from path > ... .
Then I terminated lpcxpresso and started it by double clicking on the desktop icon.
There the debugger won't launch and from path > path1.txt results an empty file, I
suppose. I have tried to upload it for reference, but this doesn't work.
During these procedures cygwin was functional again, as I had renamed it from cygwin0 back to cygwin before and forgotten about it.