LPCxpresso can not connect to the LPC LINK2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPCxpresso can not connect to the LPC LINK2

872件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by molu on Fri Oct 31 00:43:56 MST 2014
I programm from lpcxpresso to device by LPC LINK2 , but it always failed by noticed"No connection to emulator device" and as the attachment !
0 件の賞賛
4 返答(返信)

834件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Sun Nov 02 19:58:51 MST 2014
So, you need to debug your application to see what you have done to cause a Hard Fault. See

http://www.lpcware.com/content/faq/lpcxpresso/debugging-hard-fault
0 件の賞賛

834件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by molu on Sun Nov 02 19:25:30 MST 2014
sometimes it programme successfully , but jump into HardFault interrupt !
0 件の賞賛

834件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by molu on Sun Nov 02 19:02:30 MST 2014
1, It is connected ,sure .
2, power supplier is sufficient ,suer.
3, it works sometimes , so maybe the connected way is right !
0 件の賞賛

834件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by lpcxpresso-support on Fri Oct 31 02:16:29 MST 2014
It means that it cannot find the device. This could be because
[list]
  [*]- it is not connected
  [*]- it is not powered, or is not supplied with sufficient power
  [*]- the cable is connected to wrong way
  [*]- if it is a custom board, the debug circuit is designed incorrectly. See this FAQ
  [list]
  [*]http://www.lpcware.com/content/faq/lpcxpresso/debug-design
[/list]
  [*]- the device is in a bad state, preventing debug access. See this FAQ for recovery
[list]
  [*]http://www.lpcware.com/content/faq/lpcxpresso/regaining-debug-access
[/list][/list]
0 件の賞賛