When I try to debug I get the message -
LinkServer not found
When I search for Any Emulator I get nothing.
Control panel shows an MBED CMSIS-DAP and an MBED Serial PORT.
When I reset the board the GreenLED is on and when I select Debug it flashes Green/Red
I have included board.h and chip.h and tried all options in the debug configuration.
已解决! 转到解答。
Yes,many times, with a few updates
I am using OSX Seirra, running Parallels virtual machine with Windows 7.
I have the latest version of LPCXpresso.
To cut to the chase, I have found that the Avast anti-virus software had blocked one of the .exe files associates with the device driver for the board. It now works fine, but I thought I would add the extra to show that LPCXpresso can be run on a MAC and, by the way, it works fine with LPC-Link2 (I am an ex-Keil user).
Have you ever been able to debug this particular board on this specific PC? If it has worked previously, is there any obvious trigger for the problems starting - for instance an OS update, or following a debug session with a particular example?
Can you also confirm what OS and version are you running?
And what version of LPCXpresso IDE (or MCUXpresso IDE) ?
With no debug session running...
Now try launching a debug session again - preferably using one of the standard LPCOpen examples for this board - and let us know whether your debug session now suceeds.
Regards,
LPCXpresso Support
Yes,many times, with a few updates
I am using OSX Seirra, running Parallels virtual machine with Windows 7.
I have the latest version of LPCXpresso.
To cut to the chase, I have found that the Avast anti-virus software had blocked one of the .exe files associates with the device driver for the board. It now works fine, but I thought I would add the extra to show that LPCXpresso can be run on a MAC and, by the way, it works fine with LPC-Link2 (I am an ex-Keil user).
Once I realised that a file was being blocked it became quite simple to fix the problem.
1. Open Avast.
2. Click on the small BELL symbol (top right)
3. Click on "OPEN VIRUS CHEST"
4.Right click on the file that you wish to unblock and select "Restore".
5 Close all windows.