LPCXpresso IDE can't support NGX Xplorer LPC4330 Board with CMSIS-DAP Debugger

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPCXpresso IDE can't support NGX Xplorer LPC4330 Board with CMSIS-DAP Debugger

603 次查看
li-chinwang
Contributor II

  Customer wants to use LPCXpresso for cost down. I have looked the picture following.

        NGX Xplorer LPC4330 Board only support Redlink. That’s reason why function can’t work fine after I use LINK-II to program code into QSPI      Flash.

        I try to use NXP LPCXpresso4337 to download to NGX Xplorer LPC4330 Board.

        The result is I’m failed to download code to QSPI Flash.

        There is no way for customer to use LPCXpresso IDE and LINK-II right?

        If yes, what’s Redlink debugger and can let customer use LPCXpresso IDE.

        Or customer can only use Keil C to develop LPC4330?

lpc.bmp

0 项奖励
回复
1 回复

398 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

That page appears to be out-of-date. There is no problem using a CMSIS-DAP probe, such as LPC-Link2, to debug an LPC4330 from LPCXpresso IDE. For more information, please see: Which debug probes are supported by LPCXpresso IDE with which MCUs? 

Regards,

LPCXpresso Support

0 项奖励
回复