[LPCXpressoDevice_WinUSB.NTx86] %USB\LPCXpressoDevice.DeviceDesc% =USB_Install, USB\VID_1FC9&PID_0009 [LPCXpressoDevice_WinUSB.NTamd64] %USB\LPCXpressoDevice.DeviceDesc% =USB_Install, USB\VID_1FC9&PID_0009 |
dfu-util -d 0x1fc9:0x000c -c 0 -D LPC4320_Redlink_V1_03.bin.hdr |
========================= USB Port2 ========================= Connection Status : Device is connected Port Chain : 3-2 ======================== USB Device ======================== +++++++++++++++++ Device Information ++++++++++++++++++ Device Description : LPC based USB device Device ID : USB\VID_1FC9&PID_000C\ABCD Driver KeyName : {378029ad-c65d-40e3-b5fe-a740129416e4}\0000 Driver : C:\Windows\system32\DRIVERS\WinUSB.sys (Version: 6.1.7601 Date: 2010-11-20) Legacy BusType : PNPBus Class : LpcDevice Service : WinUSB Enumerator : USB Location Info : Port_#0002.Hub_#0001 Manufacturer Info : NXP Capabilities : Removable, UniqueID Address : 2 Problem Code : 0 Power State : D0 (supported: D0, D3, wake from D0) ---------------- Connection Information --------------- Connection Index : 0x02 Connection Status : 0x01 (DeviceConnected) Current Config Value : 0x01 Device Address : 0x0D Is Hub : 0x00 (no) Number Of Open Pipes : 0x00 (0) Device Bus Speed : 0x02 (High-Speed) ------------- Device Qualifier Descriptor ------------- bLength : 0x12 (18 bytes) bDescriptorType : 0x01 (Device Qualifier Descriptor) bcdUSB : 0x200 (USB Version 2.00) bDeviceClass : 0x00 (defined by the interface descriptors) bDeviceSubClass : 0x00 bDeviceProtocol : 0x00 bMaxPacketSize0 : 0x40 (64 bytes) idVendor : 0x1FC9 (NXP Semiconductors) idProduct : 0x000C bcdDevice : 0x100 iManufacturer : 0x01 Language 0x0409 : "NXP" iProduct : 0x02 Language 0x0409 : "LPC" iSerialNumber : 0x03 Language 0x0409 : "ABCD" bNumConfigurations : 0x01 -------------- Configuration Descriptor --------------- bLength : 0x09 (9 bytes) bDescriptorType : 0x02 (Configuration Descriptor) wTotalLength : 0x001B (27 bytes) bNumInterfaces : 0x01 bConfigurationValue : 0x01 iConfiguration : 0x00 bmAttributes : 0xC0 (Bus Powered, Self Powered) MaxPower : 0x32 (100 mA) ---------------- Interface Descriptor ----------------- bLength : 0x09 (9 bytes) bDescriptorType : 0x04 (Interface Descriptor) bInterfaceNumber : 0x00 bAlternateSetting : 0x00 bNumEndpoints : 0x00 bInterfaceClass : 0xFE (Application Specific) bInterfaceSubClass : 0x01 bInterfaceProtocol : 0x01 iInterface : 0x04 Language 0x0409 : "DFU" ------------------- HID Descriptor -------------------- bLength : 0x09 (9 bytes) bDescriptorType : 0x21 (HID Descriptor) bcdHID : 0x0009 (HID Version 0.09) bCountryCode : 0xFF (255 = Reserved) bNumDescriptors : 0x00 |