Content originally posted in LPCWare by ArneB on Mon Nov 14 07:17:43 MST 2011
Hi LPC freaks & experts,
I have some new ideas in my mind and i would like to discuss them with you, if it is possible or not... :)
In my next project it is not possible to connect a LPC1114 controller directly to a debug connector or something similar. But it is possible to route the SWD and reset signals to the GPIOs of a different controller, which has a physical link to a PC. I would like to use the other controller as a tunnel to my LPC controller, therefore i am able to debug/flash it from the LPCXpresso environment in the usual way.
What i need is a driver (something like the provided "crt_emu_lpc11_13_nxp.exe"), which connects the LPCXpresso IDE with my other other controller using the special physical link.
Now to my questions:
1) Is this approach possible or complete nonsense ?
2) Is there any kind of documentation available concerning the driver integration into LPCXpresso ?
3) Does anyone has any experience or perhaps even examples of such a driver ?
Thanks a lot for your help !
Arne