Change reset address on 1758

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Change reset address on 1758

645 Views
IlConte
Contributor IV

Dear all, i use 1758 and lpcxpresso  v8.1.4

I need to start application at 0x00010000 (from 0 to 0xFFFF I have bootloader)

Than my problem is start at 0x10000.

Thi is my .ld have modified  :

MEMORY
{
  /* Define each memory region */
  MFlash512 (rx) : ORIGIN = 0x00010000, LENGTH = 0x40000 /* 512K bytes (alias Flash) */  
  RamLoc32 (rwx) : ORIGIN = 0x10000000, LENGTH = 0x8000 /* 32K bytes (alias RAM) */  
  RamAHB32 (rwx) : ORIGIN = 0x2007c000, LENGTH = 0x8000 /* 32K bytes (alias RAM2) */  
}

  /* Define a symbol for the top of each memory region */
  __base_MFlash512 = 0x00010000  ; /* MFlash512 */  
  __base_Flash = 0x0 ; /* Flash */  
  __top_MFlash512 = 0x00010000 + 0x40000 ; /* 262K bytes */  
  __top_Flash = 0x0 + 0x80000 ; /* 512K bytes */  
  __base_RamLoc32 = 0x10000000  ; /* RamLoc32 */  
  __base_RAM = 0x10000000 ; /* RAM */  
  __top_RamLoc32 = 0x10000000 + 0x8000 ; /* 32K bytes */  
  __top_RAM = 0x10000000 + 0x8000 ; /* 32K bytes */  
  __base_RamAHB32 = 0x2007c000  ; /* RamAHB32 */  
  __base_RAM2 = 0x2007c000 ; /* RAM2 */  
  __top_RamAHB32 = 0x2007c000 + 0x8000 ; /* 32K bytes */  
  __top_RAM2 = 0x2007c000 + 0x8000 ; /* 32K bytes */  

When I try to start, I have the error no source found at address 0x1440 !

The correct address should be 0x11440.

My question is: why go to 0x1440 ?

The map file is correct:

 .text.ResetISR
                0x00011440       0x58 ./src/cr_startup_lpc17.o
                0x00011440                ResetISR

Thanks

0 Kudos
1 Reply

384 Views
lpcxpresso_supp
NXP Employee
NXP Employee

You could try following the mechanism described in this old FAQ - DebugThroughBootloader - ** Code Red Support Site ** .

Another approach might be to use a Linkserver (redlinkserv) reset script to set the PC "correctly" after the download to the flash. There are some example scripts in the \lpcxpresso\bin\Scripts of your tools installation. You would need to copy and then modify one of the supplied scripts, and then added a reference to the script into your launch configuration (Launch Configuration Menu ).

Regards,

LPCXpresso Support 

0 Kudos