Cannot debug NGX4330 explorer bord with 2_20 Sample Projects

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot debug NGX4330 explorer bord with 2_20 Sample Projects

686 Views
yasushiaoyama
Contributor I

Hi,

 I have been troubled in debugging NGX 4330 explore board.  Whenever I start to debug sample program (Periph_blinky), it doesn't stop at main routine.  Run - Resume command becomes in gray and not available.  I push suspend button,  the error "15: Target error from Read Memory" is displayed.

 It happens with 2_20 sample projects, but doesn't happen with 3_01 sample projects.  I found Periph_blinky in 3_01 projects debugging function work well.  But I want to use a USB host sample project, which is included in 2_20 projects but not in newest release 3_01.

 

 I'd appreciate if somebody could advice me.

Environment: LPCXpresso v8.2.2 [Build 650] [2016-09-09] 

Sample Projects: lpcopen_3_01_lpcxpresso_ngx_xplorer_4330.zip 

                          lpcopen_2_20_lpcxpresso_ngx_xplorer_4330.zip

Problem

 I Cannot debug Periph_blinky in 2_20 projects.  the error "15: Target error from Read Memory" is displayed.

 But 3_01 Periph_blinky has no problem, I can debug it.

Timeline

(1)Imported lpcopen_3_01_lpcxpresso_ngx_xplorer_4330.zip

(2)Changed memory setting of "Periph_blinky" property according to NGX 4330 Explorer manual, because LPC4330 dosn't have internal FLASH ROM.

(3)Tried to debug "Periph_blinky", I found it worked.

(4)made new work space and changed work space to the new one.

(5)Imported lpcopen_2_20_lpcxpresso_ngx_xplorer_4330.zip into new work space.

(6)Made same memory setting as I did in 3_01 project.

(7)Tried to debug "Periph_blinky", I found it didn't work.  It didn't stop at program start point, and Run-Resume command was not available.  I pushed Suspend button, the error "15: Target error from Read Memory" is displayed.

(8)Memory mapping I set is below;

<info flash_driver='LPC18_43_SPIFI_32MB_256KB.cfx'>
<chip>
<memory id='Flash' type='Flash' is_ro='true' can_program='true'></memory>
<memory id='RAM' type='RAM'></memory>
<memoryInstance id='SPIFI' derived_from='Flash' location='0x14000000' size='0x40000' edited='true' />
<memoryInstance id='RamLoc128' derived_from='RAM' location='0x10000000' size='0x20000' edited='true' />
<memoryInstance id='RamLoc72' derived_from='RAM' location='0x10080000' size='0x12000' edited='true' />
<memoryInstance id='RamAHB32' derived_from='RAM' location='0x20000000' size='0x8000' edited='true' />
<memoryInstance id='RamAHB16' derived_from='RAM' location='0x20008000' size='0x4000' edited='true' />
<memoryInstance id='RamAHB_ETB16' derived_from='RAM' location='0x2000c000' size='0x4000' edited='true' />
</chip>
</info>

  I found when problem happened, value in memory area (from 0x14000000, 0x10000000, etc.) were all "?????.." in memory widows.   

Thanks,

Yasushi Aoyama

0 Kudos
2 Replies

488 Views
lpcxpresso_supp
NXP Employee
NXP Employee

I suspect you have the wrong flash driver selected for the actual flash memory (and size) fitted on the board. Try selecting  the flash driver "LPC18_43_SPIFI_GENERIC.cfx" instead , as described in LPC18xx / LPC43xx SPIFI Flash Drivers 

You might also want to try the v2.19 LPCOpen package that ships with LPCXpresso IDE (inside the Examples subdirectory of the product install).

Regards,

LPCXpresso Support

0 Kudos

488 Views
yasushiaoyama
Contributor I

Thanks for your advice.

The first driver I tried was  "LPC18_43_SPIFI_GENERIC.cfx", but it din't work in neither 03_01 nor 02_20 projects.

Then I tried 'LPC18_43_SPIFI_32MB_256KB.cfx'  and found it works in 03_01 but not in 02_20.  Sorry I din't write it.

My interesting project is "lpcusblib_MassStorageHost". Yesterday I tried to import  the project into 03_01 project tree and was able to make it available.  So the issue became not urgent.

But I still am interesting why I cannot use 02_20 sample trees with my NGX 4330 explorer board.

Regards,

Yasushi Aoyama

 

 

0 Kudos