CLK output pin?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CLK output pin?

370 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by volter on Sat Jun 18 13:21:36 MST 2011
I need some pin to be configured as a CLK at 4MHz for my external ADC (MAX183BCNG).
Is there already build in function for this?
0 项奖励
4 回复数

352 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by volter on Sat Jun 18 14:14:24 MST 2011
I find this configuration for LPC1114 but I think it will work for LPC1343 as well
// Init
LPC_SYSCON->SYSAHBCLKCTRL |= (1<<6); // Enable GPIO clk
LPC_IOCON->PIO0_1 &= ~0x3F; // Select clkout function for P0.1

LPC_IOCON->PIO0_1 |= 0x01;

LPC_SYSCON->CLKOUTCLKSEL = 0x03; // IRC: 0x00 System osci: 0x01 WTD: 0x02 Main clk: 0x03

LPC_SYSCON->CLKOUTUEN = 0x01; // Update clock

LPC_SYSCON->CLKOUTUEN = 0x00; // Toggle update register once

LPC_SYSCON->CLKOUTUEN = 0x01;

while ( !(LPC_SYSCON->CLKOUTUEN & 0x01) ); // Wait until updated

LPC_SYSCON->CLKOUTDIV = 1; // Divided by 1

I just need to set CLKOUTDIV to 18 to get 4MHz
0 项奖励

352 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sat Jun 18 13:52:21 MST 2011

Quote: volter
OK and how I configure & use it.



Use manual of your MCU and / or read this forum?
0 项奖励

352 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by volter on Sat Jun 18 13:46:34 MST 2011

Quote: Zero
Yes,  CLKOUT :)


OK and how I configure & use it.
0 项奖励

352 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by Ex-Zero on Sat Jun 18 13:27:41 MST 2011
Yes,  CLKOUT :)
0 项奖励