Are the binaries generated by LPCXpresso different from those generated by MCUXpresso for the same Workspace?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Are the binaries generated by LPCXpresso different from those generated by MCUXpresso for the same Workspace?

1,025件の閲覧回数
mohamedshaheen
Contributor I

I opened a legacy Workspace built using LPCXpresso in MCUXpresso.  When I built the Workspace in MCUXpresso and compared the old binaries and the new binaries they were different.  Is this  the expected bahavior?

0 件の賞賛
返信
1 返信

875件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Yes. Primarily this will be because MCUXpresso IDE uses later versions of the compiler, linker and libraries than the old LPCXpresso IDE product.

Note : If you are moving projects across into MCUXpresso IDE, then I would also suggest that you read the information contained in the MCUXpresso IDE v10.1 Installation Guide : 5. Appendix B – Migrating from LPCXpresso IDE version 8.2.x – Hints and Tips

If you need further advice on this, please post to the MCUXpresso IDE community : MCUXpresso IDE 

MCUXpresso IDE Support

0 件の賞賛
返信