Are the binaries generated by LPCXpresso different from those generated by MCUXpresso for the same Workspace?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are the binaries generated by LPCXpresso different from those generated by MCUXpresso for the same Workspace?

1,022 Views
mohamedshaheen
Contributor I

I opened a legacy Workspace built using LPCXpresso in MCUXpresso.  When I built the Workspace in MCUXpresso and compared the old binaries and the new binaries they were different.  Is this  the expected bahavior?

0 Kudos
Reply
1 Reply

872 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Yes. Primarily this will be because MCUXpresso IDE uses later versions of the compiler, linker and libraries than the old LPCXpresso IDE product.

Note : If you are moving projects across into MCUXpresso IDE, then I would also suggest that you read the information contained in the MCUXpresso IDE v10.1 Installation Guide : 5. Appendix B – Migrating from LPCXpresso IDE version 8.2.x – Hints and Tips

If you need further advice on this, please post to the MCUXpresso IDE community : MCUXpresso IDE 

MCUXpresso IDE Support

0 Kudos
Reply