spifi library support for Spansion S25FL116K

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

spifi library support for Spansion S25FL116K

546 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by charchar on Wed Oct 28 07:51:41 MST 2015
Hi all,
I'm trying to get my LPC4350 to talk to the S25FL116K via spifi lib version 1.03.68 (the latest).  Looking through the source code, I noticed that this device isn't supported  in the devFamily list, although close siblings are.  I'm happy to delve into this, add support, etc, but I wanted to see if anyone has tried this (or better yet, has been successful) before I dive in. 

This part is currently the lowest-cost qspi flash out there.

thanks!
标签 (1)
0 项奖励
回复
2 回复数

482 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by charchar on Thu Oct 29 14:57:20 MST 2015
Yeah, I made some guesses and it seems to work. 
0 项奖励
回复

482 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Wed Oct 28 09:56:06 MST 2015
Hi Charchar,
It should be relatively easy to add support for this device in SPIFI library as other devices from same series are already in the lib.
Page 37 of below PDF may be helpful.
https://www.lpcware.com/system/files/lpclibspifi_1.03_68.pdf
0 项奖励
回复