eRPC for NXP LPC54605 with SPI transport

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

eRPC for NXP LPC54605 with SPI transport

ソリューションへジャンプ
2,493件の閲覧回数
sevi
Contributor II

Hi,

 

I'm looking for a convinient way to create an control and data transfer interface between the NXP MCU LPC54605 and embedded petalinux.

 

In a quick test i run into missing driver like fsl_port.h which is not available for LPC54605.

Is there a way to use eRPC with this MCU?

 

Thank you

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 解決策
2,483件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
2 返答(返信)
2,484件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
2,476件の閲覧回数
sevi
Contributor II

Hi,

 

Thank you for the answer, the information in https://github.com/EmbeddedRPC/erpc/wiki/Getting-Started were the best starting point for me.

But the problem with the missing fsl_port.h still exists. As a workaround I created an empty fsl_port.h file to be able to completely build the code.

 

Thank you and best regards

0 件の賞賛
返信