device_id of LPC11U34FBD48/311 is different from UM 10462(v5.5)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

device_id of LPC11U34FBD48/311 is different from UM 10462(v5.5)

Jump to solution
1,671 Views
helm
Contributor I

Hello.

LPC11U34FBD48/311's device_id in UM10462(v5.5) is 0x003 D440.

But my devices return 0x2000 002B.

(The address is 0x4004 83F4)

Is it right device_id ?

Or is the address wrong ?

----------

I've gotten right device_ids in some other LPC11Ux.

example)

0x2980 002B for LPC11U24FBD48/301  ( same as one in UM10462)

0x2980 102B for LPC11E14FBD48/401 ( same as one in UM10518)

-----------

Thanks.

Labels (1)
0 Kudos
1 Solution
1,637 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello helm,

Sorry I also don't know the really reason, while you can see in the " Table 48. Device ID register (DEVICE_ID, address 0x4004 83F4) bit description", there is no LPC11u3x. 

Anyway, recommend use IAP/ISP command read.

 

Thanks,

Alice

View solution in original post

0 Kudos
4 Replies
1,655 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello helm,

 

How about enter enter ISP mode using Flash Magic to read?

Or use IAP "Read Part Identification number" in your code to read?

 

BR

Alice

0 Kudos
1,647 Views
helm
Contributor I

Thanks for your reply, Alice Yang.

I tried ISP and IAP.

I got the right device_id(0x003 D440) with the ISP mode command "J" and the right one with IAP command 54.

Thank you.

 

However, the right address of device_id is 0x4004 83F8 not 0x4004 83F4.

actual data::

0x400483f4: 2b 00 00 20 40 d4 03 00

Is the address changeable depending on product's Lot in LPC11Uxx ?

 

Regards,

Helm

 

 

0 Kudos
1,638 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello helm,

Sorry I also don't know the really reason, while you can see in the " Table 48. Device ID register (DEVICE_ID, address 0x4004 83F4) bit description", there is no LPC11u3x. 

Anyway, recommend use IAP/ISP command read.

 

Thanks,

Alice

0 Kudos
1,632 Views
helm
Contributor I

Certainly there is no LPC11U3x in Table 48 as you say.

It's a little bit difficult notation because of the description;

"This device ID register is a read-only register and contains the part ID for each LPC11U3x/2x/1x part."

in 3.5.42 of UM10462.

 

Anyway, I will use ISP/IAP for detecting DEVICE_ID.

Thanks !

 

I attach a link I found today for other's reference.

https://community.nxp.com/t5/LPC-Microcontrollers/LPC11U68JBD100-Device-ID/m-p/537085 

 

Regards,

Helm

 

 

0 Kudos