PN5180开发板的P2P模式

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN5180开发板的P2P模式

1,364件の閲覧回数
2468645898
Contributor II
您好, 我想问一下,PN5180开发对应的SDK——NFC Reader Library v4.040.05.011646 R1 for PNEV5180B including all software examples中的NfcrdlilbEx3_NFCForum示例关于18092主动通信作为发起端时为什么106k速率部分的代码是空的呢?是因为PN5180不支持这一速率下的通信?还是应用中不会用到这一速率下的P2P?还是其它原因呢? 麻烦您尽快回复一下,谢谢!
0 件の賞賛
4 返答(返信)

1,336件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

楼主:

您好,你提供的这段代码我在NFC library v6.0中好像没找到。您可以下载最新版的library再确认一下。

希望能够帮助到您。

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛

1,340件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

楼主:

您好,您这个问题和在NFC team 提交的问题是同一个问题。我们将解答你在NFC team 提交的问题。

谢谢您的理解。

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛

1,338件の閲覧回数
2468645898
Contributor II

@fangfang 谢谢您,麻烦尽快回答一下

0 件の賞賛

1,362件の閲覧回数
2468645898
Contributor II

2468645898_0-1617955067560.png

 

0 件の賞賛