NO FLASH ALGORITHM  FOR : 000002FCh - 000002FFh

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NO FLASH ALGORITHM  FOR : 000002FCh - 000002FFh

476 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by SHEKAR MJ on Wed Jun 04 05:34:08 MST 2014
while programming through JTAG to external flash it is showing No flash algorithum found for 000002FCh - 000002FFh. Controller not programming.See the attached image.
Labels (1)
0 Kudos
2 Replies

432 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by SHEKAR MJ on Wed Jun 04 21:23:51 MST 2014
Hi mc

Thanks for your reply.

Summary of my project.
          Earliar we were using LPC2420 Controller with external flash SST39vf1601 and our code size is nearly 1.2MB. Since LPC1777 is direct replacement for LPC24XX series, in the same board we are planning to change only controller(LPC1777).  Because of code size we have to use external flash for programming and booting. We have successfully added the flash programming algorithm in keil.

          we are using Chip select 1 for SST flash we made the target settings according to that. Please refer the attached image. Now while programming through ULINK2 JTAG, Full chip erasing is happening properly and Partial programming is also happening. But it is showing no algorithm found for 0x000002FC to 0x000002FF. This address is related to CRP. Please help us to overcome this issue and move forward.

Regards
Shekar


0 Kudos

432 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Wed Jun 04 10:43:07 MST 2014
Hi Shekar MJ,
Can you show your target setting? Looks like settings in target tab of option dialog box are not correct.
0 Kudos