Hi !
Unfortunately flash memory can be written by 512 bytes chunks only.
But I need to sabe small 16-128 bytes chunks and I can see I can read modify and write the same page several times.
LPC55S69 flash memory has erased state as 0x00 and each bit can be programmed to 1 on time.
So I can program page several time but I can only modify bit 0 to bit 1 and not wise versa what is typical for flash memory technology.
But each type of memory have clear limit of NOP operations what can be done on one page before Erase must be executed ( What's NOPs of NAND as example ).
What amount of NOP's are specified for that flash memory what is part of LPC55S69 MCU ?
Regards,
Eugene
Eugene,
I guess you ask Flash endurance parameter. see below table, it is extracted from LPC55S6X datasheet.
Have a great day,
Jun Zhang
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi !
Not it is not endurance , this is partial write e.h how may times you can write one 512 pages before erase.
e.g read whole page ( if need ) fill some area and write back. During this operation you can change only bits from 1 to 0 or may be like in your case 0 to 1 only.
But each type of memory must have this value, It can be 1 as well. Too much overwrite cause retention problems for sure.
OR I can write 512 one time and after that only erase must be done. In other case you might not garantie data retention at all.
But NXP should specify this value. In other case is very difficult to implement any file system on top of LPC's flash memory.
Regards,
Eugene
Hi !
For example here : NOR Flash FAQs - KBA222273 | Cypress Developer Community
"
Is it possible to write twice (erase → write → write to the same address) without reissuing the Erase command for the same address?
It is physically possible to change 1→0, but if you write to the same Write Page twice, the built-in ECC function will be invalid. So, it is not recommended to write twice.
"
So in NXP , I don't know how you calculate ECC ans etc. But this value is essential for implement compact flash file systems on top of some types of memory.
br, Eugene
Hi,
LPC55S69 doesn't define NOP value.
But the flash program principle is, after erase, physically program from 0->1, no way to do it vice versa if using Flash program command.
Have a great day,
Jun Zhang
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi ZhangJennie !
So I can write page one time or multiple time for keep rule 0->1 and ECC of page will be updated automatically and no data retention degradation ?
Or NXP forbid to write several times ?
Regards,
Eugene
can this question be asked from silicon manufacture part of NXP for be sure if current process of flash memory supports this kind of operation without degradation of endurance and retention capabilities of used flash memory
For the data that are not documented, mostly two reasons: no test on it, or can't share to public.
If we want to request it, we need more information from you so that I can compose my internal request:
- your project name and scenarios
- the sufficient reason why you need these data
- the chips ordered yearly.
- company name.
the market will evaluate and make decision if we have resource to arrange the test.
Hi !
No need any testing. Every memory vendor always specify this value or clearly said how-to write data to the sector.
In other case it is internal flash memory for firmware code only and it shouldn't be used for store any data in any fashions.
Regards,
Eugene
To complement this thread:
It is a valid question, but in the case of the LPC55XX there is another reason to avoid over-programming:
From chapter 5.7.13 of the User's Manual
Due to the presence of ECC, over-programming an already programmed word will likely result in inconsistent parity bits; for this reason, it is not allowed to program a memory word without erasing it first.
Anyway, programming smaller portions of data into the flash is possible, the 512 bytes pages don't play a role for writing. Data word can be written in 128 bit format, so four 32-bit word are the smallest portion which can be written to the flash
From chapter 5.7.8 of the User's Manual:
Data to be written is accumulated inside the controller’s DATAW0-DATAW3 registers. After specifying an address in the STARTA register and 128 bit of data in the DATAW0-3 registers, it’s possible to activate the controller’s Write” command, which will transfer the data to the memory’s page register, at the position indicated by the STARTA register (only the column part of the address is significant).
However, erasing is bound to the 512-byte pages, so even for small parameter sections you need two pages to swap between them, even if the content is just a few bytes.
Regards,
Bernhard.
Hi bernhardfink !
But NXP doesn't provide any API's for manipulate with smaller chunks what is less than 512 bytes,
In my case I have multiple 128 bytes chunks what I would like to compact in one page sequentially.
Noe I should do read-modify-write operation for 512 byte window,
Or possible to control FLASH controller directly and this part can be added to SDK ?
Regards,
Eugene
Hi Eugene,
I need to admit that i didn't look at this on API level.
If a programming cycle can only take place on a page, then you need to switch between two pages and do it in 3 steps:
We don't provide more details about the flash controller, so you need to live with the functionality provided by the API.
Regards,
Bernhard.