LPC55S69 keil编译问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69 keil编译问题

1,801 Views
haifeng_jin
Contributor III

在编译LPC55S69的SDK出现如下问题,pack都是安装的,不知道是什么问题,有遇到过吗

ArmClang: error: ARM Compiler does not support '-mcpu=cortex-m33'

pastedImage_1.png

Labels (1)
0 Kudos
Reply
4 Replies

1,604 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  haifeng jin,

Yes, as sean said, you need Professional license.

Do you still have question about this? 

0 Kudos
Reply

1,604 Views
robertboys
Contributor IV

Hello

Starting with Keil MDK 5.31, a MDK Pro license will not be needed for Armv8-M (Cortex-M23, M33, and so on).

Other versions of MDK will work with these TrustZone processors.

Even MDK-Lite (the evaluation version) will work to 32K.

MDK 5.31 is expected to be released early July 2020.

I just updated my LPC55S69 lab:   www.keil.com/appnotes/docs/apnt_322.asp

0 Kudos
Reply

1,604 Views
haifeng_jin
Contributor III

ok,谢谢,确实是licensec问题

0 Kudos
Reply

1,604 Views
seanzhou
Contributor II

LPC55 is ARM V8 cortex m33.

You need professional Keil version to compile it.

0 Kudos
Reply