LPC55S28 Oscillator Requirements with High Speed USB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPC55S28 Oscillator Requirements with High Speed USB

跳至解决方案
541 次查看
zach890
Contributor I

I'm working on a new design with the LPC55S28 that will be utilizing high speed USB for data connections. Reading the data sheet and the user guide it's not completely clear what the external oscillator requirements are for the chip.

Both the data sheet and the user guide refer to the high speed USB clock as the 16MHz clock but section 45 (USB Phy) of the user guide mentions that XO32M can be configured to 16, 19.2, 20, 24, or 32MHz. Does this mean that an external crystal oscillator can operate at any of those frequencies or does it have to be 16MHz? Alternatively is an external oscillator needed for high speed USB the datasheet and user guide implies that it is a requirement.

Thanks for the help!

标签 (2)
标记 (2)
0 项奖励
1 解答
528 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

"Does this mean that an external crystal oscillator can operate at any of those frequencies"

->> Yes.

 

 

在原帖中查看解决方案

0 项奖励
1 回复
529 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

"Does this mean that an external crystal oscillator can operate at any of those frequencies"

->> Yes.

 

 

0 项奖励