LPC5536 I3C NO WORK----USE LPC55S36 SAMPLE CODE I3C SENSOR NET WORK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC5536 I3C NO WORK----USE LPC55S36 SAMPLE CODE I3C SENSOR NET WORK

Jump to solution
1,705 Views
luna_liang
Contributor II

DEARS,

I used LPCXpresso55S36 test i3c port,use i3c port PIN 69,PIN 55, no clock and data.please help check if the demo is OK,or please help share a project about I3C TO USB application ,thank you.

luna_liang_0-1710315891456.png

 

0 Kudos
Reply
1 Solution
1,684 Views
HangZhang
NXP Employee
NXP Employee

Hi @luna_liang 

I downloaded SDK_2_10_2_LPCXpresso55S36, and run the i3C master_read_sensor_icm42688p example. It can work.

Please note the readme in the example.

Image (6).jpg

I hope can help you.

Best regards,
Hang

 

View solution in original post

0 Kudos
Reply
9 Replies
1,685 Views
HangZhang
NXP Employee
NXP Employee

Hi @luna_liang 

I downloaded SDK_2_10_2_LPCXpresso55S36, and run the i3C master_read_sensor_icm42688p example. It can work.

Please note the readme in the example.

Image (6).jpg

I hope can help you.

Best regards,
Hang

 

0 Kudos
Reply
1,673 Views
luna_liang
Contributor II

now download is 2_15 ,please help share 2_10 SDK,thank you.

Tags (1)
0 Kudos
Reply
1,673 Views
luna_liang
Contributor II
现在下载的都是2_15版本的例程,能分享你的2_10吗
0 Kudos
Reply
1,671 Views
HangZhang
NXP Employee
NXP Employee

Hi @luna_liang 

您好,

请您在官网如图选择2.10 SDK 下载。

HangZhang_0-1710404437852.png

谢谢

 

0 Kudos
Reply
1,641 Views
luna_liang
Contributor II

麻烦给一下您邮箱,thank you。

0 Kudos
Reply
1,644 Views
luna_liang
Contributor II

luna_liang_0-1710469173264.png

2.10.2这个工程只有这个工程,选项里有I2C,没看到I3C module

这个是可以用吗

0 Kudos
Reply
1,631 Views
luna_liang
Contributor II

dear hang,

thank you,my demo has no R554,had read the read me doc,this need a short connect in R554_ PIN 2 TO PIN3,

SO can not run sussesful . 

only to print: I3C master do dynamic address assignmentto the sensor slave.

0 Kudos
Reply
1,604 Views
Alex_Wang
NXP Employee
NXP Employee

Hi @luna_liang 

You can download the 2.10.2 SDK by following the steps in the video.

Best regards, Alex

0 Kudos
Reply
1,616 Views
HangZhang
NXP Employee
NXP Employee

Hi @luna_liang

你下载的应该是2.15的SDK,2.10的里面没有R554。

 下图为下载的压缩包,和 read me。我会邮箱发给你该压缩包。

HangZhang_0-1710490930227.pngHangZhang_1-1710490979233.png

 

0 Kudos
Reply