Do you have some sample project to flash LPC54018JxM’s internal flash?
I’ve downloaded full 54S018M::SDK 2.5.0 but could not find any example.
While browsing SDK builder’s standalone examples for 54S018M; I stumbled upon and downloaded “flashloader” (targeting KEIL IDE); however there is no readme file and the project does not compile, I get the errors below. Please advise.
>>>
*** Using Compiler 'V5.06 update 4 (build 422)', folder: 'C:\Keil_v5\ARM\ARMCC\Bin'
Rebuild target 'flashloader release'
compiling external_memory_property_map_LPC54S018M.c...
LPC54S018M/external_memory_property_map_LPC54S018M.c(8): error: #5: cannot open source input file "property/property.h": No such file or directory
#include "property/property.h"
LPC54S018M/external_memory_property_map_LPC54S018M.c: 0 warnings, 1 error
compiling bl_flexcomm_spi_irq_config_common.c...
LPC54S018M/bl_flexcomm_spi_irq_config_common.c(8): error: #5: cannot open source input file "bootloader/bl_context.h": No such file or directory
#include "bootloader/bl_context.h"
LPC54S018M/bl_flexcomm_spi_irq_config_common.c: 0 warnings, 1 error
compiling bl_flexcomm_usart_irq_config_common.c...
LPC54S018M/bl_flexcomm_usart_irq_config_common.c(8): error: #5: cannot open source input file "bootloader/bl_context.h": No such file or directory
#include "bootloader/bl_context.h"
LPC54S018M/bl_flexcomm_usart_irq_config_common.c: 0 warnings, 1 error
compiling bl_flexcomm_i2c_irq_config_common.c...
LPC54S018M/bl_flexcomm_i2c_irq_config_common.c(8): error: #5: cannot open source input file "bootloader/bl_context.h": No such file or directory
#include "bootloader/bl_context.h"
LPC54S018M/bl_flexcomm_i2c_irq_config_common.c: 0 warnings, 1 error
compiling memory_map_LPC54S018M.c...
LPC54S018M/memory_map_LPC54S018M.c(8): error: #5: cannot open source input file "bootloader/bl_context.h": No such file or directory
#include "bootloader/bl_context.h"
LPC54S018M/memory_map_LPC54S018M.c: 0 warnings, 1 error
compiling peripherals_LPC54S018M.c...
LPC54S018M/peripherals_LPC54S018M.c(8): error: #5: cannot open source input file "bootloader/bl_context.h": No such file or directory
#include "bootloader/bl_context.h"
LPC54S018M/peripherals_LPC54S018M.c: 0 warnings, 1 error
compiling key_store_hal_lpc54s018.c...
source/authentication/src/key_store_hal_lpc54s018.c(8): error: #5: cannot open source input file "bootloader/bl_context.h": No such file or directory
#include "bootloader/bl_context.h"
source/authentication/src/key_store_hal_lpc54s018.c: 0 warnings, 1 error
compiling bl_app_crc_check.c...
source/bootloader/src/bl_app_crc_check.c(8): error: #5: cannot open source input file "utilities/fsl_assert.h": No such file or directory
#include "utilities/fsl_assert.h"
source/bootloader/src/bl_app_crc_check.c: 0 warnings, 1 error
compiling bl_context.c...
source/bootloader/src/bl_context.c(9): error: #5: cannot open source input file "bootloader/bl_context.h": No such file or directory
#include "bootloader/bl_context.h"
source/bootloader/src/bl_context.c: 0 warnings, 1 error
compiling autobaud_irq.c...
source/autobaud/autobaud_irq.c(9): error: #5: cannot open source input file "autobaud/autobaud.h": No such file or directory
#include "autobaud/autobaud.h"
source/autobaud/autobaud_irq.c: 0 warnings, 1 error
compiling bl_main.c...
source/bootloader/src/bl_main.c(11): error: #5: cannot open source input file "utilities/fsl_assert.h": No such file or directory
#include "utilities/fsl_assert.h"
source/bootloader/src/bl_main.c: 0 warnings, 1 error
compiling clock_config_LPC54S018M.c...
LPC54S018M/clock_config_LPC54S018M.c(9): error: #5: cannot open source input file "bootloader/bl_context.h": No such file or directory
#include "bootloader/bl_context.h"
LPC54S018M/clock_config_LPC54S018M.c: 0 warnings, 1 error
compiling hardware_init_LPC54S018M.c...
LPC54S018M/hardware_init_LPC54S018M.c(9): error: #5: cannot open source input file "bootloader/bl_context.h": No such file or directory
#include "bootloader/bl_context.h"
LPC54S018M/hardware_init_LPC54S018M.c: 0 warnings, 1 error
compiling bl_command.c...
source/bootloader/src/bl_command.c(10): error: #5: cannot open source input file "bootloader/bootloader.h": No such file or directory
#include "bootloader/bootloader.h"
source/bootloader/src/bl_command.c: 0 warnings, 1 error
compiling pinmux_utility_lpc.c...
LPC54S018M/pinmux_utility_lpc.c(12): error: #5: cannot open source input file "bootloader/bl_context.h": No such file or directory
#include "bootloader/bl_context.h"
LPC54S018M/pinmux_utility_lpc.c: 0 warnings, 1 error
compiling bl_misc.c...
source/bootloader/src/bl_misc.c(8): error: #5: cannot open source input file "bootloader/bootloader.h": No such file or directory
#include "bootloader/bootloader.h"
source/bootloader/src/bl_misc.c: 0 warnings, 1 error
compiling system_LPC54S018M.c...
compiling fsl_power.c...
compiling fsl_reset.c...
compiling fsl_common.c...
compiling fsl_inputmux.c...
compiling bl_shutdown_cleanup.c...
source/bootloader/src/bl_shutdown_cleanup.c(10): error: #5: cannot open source input file "utilities/fsl_rtos_abstraction.h": No such file or directory
#include "utilities/fsl_rtos_abstraction.h"
source/bootloader/src/bl_shutdown_cleanup.c: 0 warnings, 1 error
compiling bl_tree_root.c...
source/bootloader/src/bl_tree_root.c(9): error: #5: cannot open source input file "bootloader/bootloader.h": No such file or directory
#include "bootloader/bootloader.h"
source/bootloader/src/bl_tree_root.c: 0 warnings, 1 error
compiling fsl_crc.c...
compiling key_store.c...
compiling flexcomm_i2c_peripheral_interface.c...
source/bootloader/src/flexcomm_i2c_peripheral_interface.c(10): error: #5: cannot open source input file "bootloader/bl_context.h": No such file or directory
#include "bootloader/bl_context.h"
source/bootloader/src/flexcomm_i2c_peripheral_interface.c: 0 warnings, 1 error
compiling bl_exception_handler.c...
compiling fsl_flexcomm.c...
compiling fsl_power_lib.c...
compiling fsl_puf.c...
compiling flexcomm_spi_peripheral_interface.c...
source/bootloader/src/flexcomm_spi_peripheral_interface.c(9): error: #5: cannot open source input file "utilities/fsl_assert.h": No such file or directory
#include "utilities/fsl_assert.h"
source/bootloader/src/flexcomm_spi_peripheral_interface.c: 0 warnings, 1 error
compiling fsl_usart.c...
compiling flexcomm_usart_peripheral_interface.c...
source/bootloader/src/flexcomm_usart_peripheral_interface.c(9): error: #5: cannot open source input file "bootloader/bl_context.h": No such file or directory
#include "bootloader/bl_context.h"
source/bootloader/src/flexcomm_usart_peripheral_interface.c: 0 warnings, 1 error
compiling usb_osa_bm.c...
compiling usb_hid_msc_peripheral_interface.c...
source/bootloader/src/usb_hid_msc_peripheral_interface.c(9): error: #5: cannot open source input file "bootloader/bl_context.h": No such file or directory
#include "bootloader/bl_context.h"
source/bootloader/src/usb_hid_msc_peripheral_interface.c: 0 warnings, 1 error
compiling crc32.c...
source/crc/crc32.c(8): error: #5: cannot open source input file "crc/crc32.h": No such file or directory
#include "crc/crc32.h"
source/crc/crc32.c: 0 warnings, 1 error
compiling crc16.c...
source/crc/crc16.c(8): error: #5: cannot open source input file "crc/crc16.h": No such file or directory
#include "crc/crc16.h"
source/crc/crc16.c: 0 warnings, 1 error
compiling bl_user_entry.c...
compiling fsl_spi.c...
compiling fsl_i2c.c...
compiling normal_memory.c...
source/memory/src/normal_memory.h(10): error: #5: cannot open source input file "memory/memory.h": No such file or directory
#include "memory/memory.h"
source/memory/src/normal_memory.c: 0 warnings, 1 error
compiling device_memory.c...
source/memory/src/device_memory.h(10): error: #5: cannot open source input file "memory/memory.h": No such file or directory
#include "memory/memory.h"
source/memory/src/device_memory.c: 0 warnings, 1 error
compiling aes_otp.c...
compiling fsl_gpio.c...
compiling sram_init_lpc.c...
source/memory/src/sram_init_lpc.c(9): error: #5: cannot open source input file "bootloader/bl_context.h": No such file or directory
#include "bootloader/bl_context.h"
source/memory/src/sram_init_lpc.c: 0 warnings, 1 error
compiling fsl_gint.c...
compiling fsl_clock.c...
assembling pattern_fill.s...
compiling microseconds_sysclk.c...
source/drivers/microseconds/microseconds_sysclk.c(150): error: #20: identifier "__WEAK" is undefined
__WEAK uint32_t microseconds_get_clock(void)
source/drivers/microseconds/microseconds_sysclk.c(150): error: #101: "uint32_t" has already been declared in the current scope
__WEAK uint32_t microseconds_get_clock(void)
source/drivers/microseconds/microseconds_sysclk.c(150): error: #65: expected a ";"
__WEAK uint32_t microseconds_get_clock(void)
source/drivers/microseconds/microseconds_sysclk.c(164): warning: At end of source: #12-D: parsing restarts here after previous syntax error
source/drivers/microseconds/microseconds_sysclk.c: 1 warning, 3 errors
compiling serial_packet.c...
source/packet/src/serial_packet.c(10): error: #5: cannot open source input file "bootloader/bl_context.h": No such file or directory
#include "bootloader/bl_context.h"
source/packet/src/serial_packet.c: 0 warnings, 1 error
compiling sbloader.c...
source/sbloader/src/sbloader.c(12): error: #5: cannot open source input file "sbloader/sbloader.h": No such file or directory
#include "sbloader/sbloader.h"
source/sbloader/src/sbloader.c: 0 warnings, 1 error
compiling spifi_nor_memory.c...
source/memory/src/spifi_nor_memory.c(9): error: #5: cannot open source input file "bootloader/bootloader.h": No such file or directory
#include "bootloader/bootloader.h"
source/memory/src/spifi_nor_memory.c: 0 warnings, 1 error
compiling property_lpc.c...
source/property/src/property_lpc.c(10): error: #5: cannot open source input file "property/property.h": No such file or directory
#include "property/property.h"
source/property/src/property_lpc.c: 0 warnings, 1 error
compiling memory.c...
source/memory/src/memory.c(10): error: #5: cannot open source input file "bootloader/bl_context.h": No such file or directory
#include "bootloader/bl_context.h"
source/memory/src/memory.c: 0 warnings, 1 error
compiling fsl_assert.c...
source/utilities/src/fsl_assert.c(8): error: #5: cannot open source input file "utilities/fsl_rtos_abstraction.h": No such file or directory
#include "utilities/fsl_rtos_abstraction.h"
source/utilities/src/fsl_assert.c: 0 warnings, 1 error
compiling fsl_rtos_abstraction.c...
source/utilities/src/fsl_rtos_abstraction.c(8): error: #5: cannot open source input file "utilities/fsl_assert.h": No such file or directory
#include "utilities/fsl_assert.h"
source/utilities/src/fsl_rtos_abstraction.c: 0 warnings, 1 error
compiling fsl_spifi.c...
compiling otp.c...
assembling startup_LPC54S018M.s...
compiling fsl_pint.c...
compiling startup.c...
compiling hid_bootloader.c...
source/usb/bm_composite/hid_bootloader.h(13): error: #5: cannot open source input file "utilities/fsl_rtos_abstraction.h": No such file or directory
#include "utilities/fsl_rtos_abstraction.h"
source/usb/bm_composite/hid_bootloader.c: 0 warnings, 1 error
compiling msc_disk.c...
source/usb/bm_composite/msc_disk.c(18): error: #5: cannot open source input file "sbloader/sbloader.h": No such file or directory
#include "sbloader/sbloader.h"
source/usb/bm_composite/msc_disk.c: 0 warnings, 1 error
compiling composite.c...
source/usb/bm_composite/hid_bootloader.h(13): error: #5: cannot open source input file "utilities/fsl_rtos_abstraction.h": No such file or directory
#include "utilities/fsl_rtos_abstraction.h"
source/usb/bm_composite/composite.c: 0 warnings, 1 error
compiling usb_descriptor.c...
source/usb/bm_composite/bootloader_hid_report_ids.h(10): error: #5: cannot open source input file "packet/command_packet.h": No such file or directory
#include "packet/command_packet.h"
source/usb/bm_composite/usb_descriptor.c: 0 warnings, 1 error
compiling spifi_nor_flash.c...
compiling usb_device_msc_ufi.c...
compiling usb_device_msc.c...
compiling usb_device_hid.c...
compiling usb_device_class.c...
compiling usb_device_ch9.c...
compiling usb_device_dci.c...
compiling usb_device_lpcip3511.c...
"release\flashloader.out" - 41 Error(s), 1 Warning(s).
Target not created.
Build Time Elapsed: 00:00:05
Hi bob belmont ,
Thank you for your interest in NXP Semiconductor products and
for the opportunity to serve you.
It seems a bit weird.
The flashloader demo is compiled well on my site, my Keil is 5.24.1.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
I use KEIL 5.22.0.0. Please see attached version of the flashloader.zip I downloaded. It looks like the project's is missing some include path.
Is there a "readme" file on how to use the app ? Is this intended to work with LPC54018JxM's 4MB internal flash ?
it does not appear to be, because of the following configuration item in bootloader_config.h
#define BL_FEATURE_HAS_NO_INTERNAL_FLASH (1)
but without any documentation it's hard for me to figure out how to use this firmware.This application appears to rely on a host application to feed it with command and data ? if so which one ?
I am looking for an example to flash LPC54018JxM's internal 4MB flash. Please help.
Edit: I believe I figured it out. flashloader is part of the mcu_boot tool chain. I downloaded the full SDK with mcu_boot option checked, and the resulting flashloader (SDK\lpcxpresso54s018m\bootloader_examples) does compile under KEIL V 5.22.0.0 w/o errors.
The standalone example (that one may download via SDK dashboard) that I've attached in my previous post is miss configured and does not compile.