LPC51U68 min USB VDD 3V

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC51U68 min USB VDD 3V

439 次查看
jh0
Contributor IV

Hi,

Is there any way to use LPC51U68 USB with 1.8V VDD. If not, is there any similar device (M0+ 100MHz) with this possibility.

标签 (1)
0 项奖励
回复
2 回复数

342 次查看
soledad
NXP Employee
NXP Employee

Yes, the LPC51U68 it is one self-power supply, as you can review in the datasheet of the device Section 13.6 Suggested USB Interface Solutions.

Best Regards,

TIC Support Team

0 项奖励
回复

342 次查看
jh0
Contributor IV

In Section 13.6 fig 33 VBUS(1) is combination that I want. Question is if in case of VDD=1.8V USB (CDC device) can work or not? Because in table 12 (10.1 General operating conditions) there is min 3.0V VDD specified for USB operation only!

0 项奖励
回复