大家好:
我正在使用LPC51U68进行项目开发,目前正在调试IAP功能,因为是第一次开发这个功能,所以有几个问题想要得到帮助,如下:
1.我之前看了很多关于IAP的信息,同时也使用了官方提供的例程,学会了内部Flash的擦写,但是我不知道如何进行boot与应用程序之间的相互跳转,我是想应用程序从0x8000(扇区1)处开始,boot程序从0x0开始。
2.重映射功能该如何实现,我查到需要对VTOR 寄存器操作,但是我并没有在UM11071的手册上找到这个寄存器的介绍,请问这个寄存器的介绍在哪里,或者说我应该怎么操作才能实现重映射? 下面是官方程序中的代码。
非常感谢各位的帮助
Hi 云龙 赵,
非常感谢使用NXP产品,很高兴为你提供技术支持!
1.我之前看了很多关于IAP的信息,同时也使用了官方提供的例程,学会了内部Flash的擦写,但是我不知道如何进行boot与应用程序之间的相互跳转,我是想应用程序从0x8000(扇区1)处开始,boot程序从0x0开始。
-- 建议参考LPC11U68的bootloader应用相关手册,因为目前LPC51U68没有对应的应用手册,他们俩都是基于Coretex-M0+核的,所以具有可参考性,链接如下:
Scalable Entry Level 32-bit Microcontroller (MCU) based on Arm® Cortex®-M0+ and Cortex®-M0 Cores | N...
2.重映射功能该如何实现,我查到需要对VTOR 寄存器操作,但是我并没有在UM11071的手册上找到这个寄存器的介绍,请问这个寄存器的介绍在哪里,或者说我应该怎么操作才能实现重映射? 下面是官方程序中的代码。
-- 关于VTOR寄存器的介绍,请参考The Definitive Guide to
ARM® Cortex®-M0 and Cortex-M0+ Processors, 因为这是Cortex-M核内部的寄存器。
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
非常感谢,我看了M0+的手册后,找到了VTOR寄存器,并且在UM11071上找到了关于重映射的内容,手册的下载地址是https://www.nxp.com.cn/webapp/sps/download/preDownload.jsp?render=true。其中3.5章应该是介绍这个的,但是我不明白应该如何修改,我使用的是keil,不知道imageHeader相关的定义该如何设置?
再次表示感谢~~
Hi 云龙 赵,
感谢回复。
你想修改imageHearder内的什么值来说实现什么样功能或目的呢?
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi 云龙 赵,
感谢回复。
目前,LPC51U68不支持此功能。
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi 云龙 赵,
感谢回复。
IAP没有指令是实现bootloader跳转到application功能的,具体IAP指令功用,
请参考手册里面的介绍。
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------