LPC1788 EA Board + Display "7 800x480

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC1788 EA Board + Display "7 800x480

435 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by embtech on Mon Nov 07 13:49:20 MST 2011
Help me,

I am trying to use emWin with LPC1788 EA Board + Display "7 800x480 EA.
Exists preconfigured package for this.

How do I change the example included in the installer NXP_emWin512_EA1788_320240_260911.zip to work with this display
Has anyone done this?


link display: http://www.embeddedartists.com/products/displays/lcdb_70.php
link EA Board: http://www.embeddedartists.com/products/kits/lpc1788_kit.php

Best regards,
Renato
标签 (1)
0 项奖励
2 回复数

407 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by zavataafnan on Fri Dec 30 00:29:11 MST 2011
Is is possible to change the code for LCD 3.2 inch to support the LCD 7 inch? Is it easy or Not?
couple of weeks means how many weeks?

Best Regards,
MJM
0 项奖励

407 次查看
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by ktownsend on Thu Dec 15 14:56:45 MST 2011
There should be an update for the LPC1788 to also support the 4.3" and 7" displays in the next couple weeks.  It will be posted on the website here as soon as it is finished and tested.
0 项奖励