LPC1768 Keil Board (MCB1700) best way to switch to WiFi ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1768 Keil Board (MCB1700) best way to switch to WiFi ?

543件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by cell85 on Tue Nov 20 08:43:26 MST 2012
Hi,

I developed a Energymeter on my MCB1700 from Keil(LPC1786). I'm using a Webinterface to visualize how much Energy my house is loosing due usage of old Washingmachines, freezers etc.
Everything works finde with the LAN on-Board.

I now want to switch to Wifi and I don't want to use a Wifi-bridge connected to the Lan-Port or something.
Is there a Wifi module which I could easily add to the board or replace with the LAN-Phy?  (Yes i want to design a new PCB)

I would appreciate your help guys.

regards
Sven
ラベル(1)
0 件の賞賛
返信
1 返信

502件の閲覧回数
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by bigkahuna on Sun Nov 25 19:21:19 MST 2012
What is the data rate you are going to need?
What is the wireless band you could use safely in your country?
What is the distance that wireless signal has to travel?
If you need something to experiment with, best to look for ZigBee board available from Sparkfun.com.  Low datarate, long distances, very easy to interface with using AT commands and cheap as any wireless boards can get.
0 件の賞賛
返信