LPC11u68 Expresso Board Hold Pin Low During Power Up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC11u68 Expresso Board Hold Pin Low During Power Up

747 Views
dustinhagstrom
Contributor I

Hello all, 

I have an LPC11u68 LpcExpresso board and I have uploaded the attached cpp file (via creating a new project and verifying it runs correctly).  My program wishes to hold a pin low even through power cycles of the LPC board.  As you can see from the attached sketch I have put a pulldown via pin muxing on pin 1_18 and I tell the system to make it output low.

The problem is, when I power up the board there is a very brief period where the pin goes high just as the power goes high, then the pin goes low as it should.  Is there a way to keep that pin low even during power application to the board?  It is a requirement for a project I am working on.  

In the attached scope shot, the (Yellow) Channel 1 is pin 1_18 and the (Blue) Channel 2 is the 3.3V line to show when power is applied.

Thank you for your help,

Dustin

Labels (1)
Tags (1)
0 Kudos
1 Reply

656 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Dustin Hagstrom,

To update this case, please reply to this email.
Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.

It's no way to modify the default state of pin: pull-up enabled before execute the corresponding instruction.

Hope this is clear.

TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos