Hitex LPC1850 evaluation board------reconfig SPIFI speed and lpc18xx-2013-09-04[1].zip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hitex LPC1850 evaluation board------reconfig SPIFI speed and lpc18xx-2013-09-04[1].zip

436 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by robert on Fri Dec 06 01:17:13 MST 2013
Dears,

Now we use the Hitex LPC1850 evaluation board: LPC1850FET256P6G566.04 ESD11460AY, and SPANSION FL064P1F 1059030. We find there is two problem:
1.use the NXP 2012-06 level-II training code:HOT7_SPIFI, if we reconfig the SPIFI colock, when simulate and debug, the MCU will entry HardFault_Handler; when run in SPI Flash, will dead, maybe also entry HardFault_Handler. Why?  SPI flash problem, or library or ROM code/library compatibility ?

2.download the lpc18xx-2013-09-04[1].zip code, use uart polling example code, then find the Baud rate is not right, becaue the pc receive date is messy code. why?

Thanks and Best regards
Robert
Labels (1)
0 Kudos
5 Replies

411 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Mon Dec 16 10:43:00 MST 2013
Hi Robert,
You can debug the reason of hard fault. Go to
Peripheral Menu -> Core Peripheral -> Fault Reports

After this you will see the register as in  the attached PNG file.

If you still can not debug Please post your project here.


0 Kudos

411 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by robert on Wed Dec 11 19:44:32 MST 2013
Dear MC,

Yes , i run the code in RAM.
0 Kudos

411 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Wed Dec 11 07:46:23 MST 2013
Hi Robert,
Please run routine from RAM which are modifying SPIFI clock (QSPI clock). Changing SPIFI clock while executing from QSPI flash will create problems.
0 Kudos

411 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by robert on Sun Dec 08 19:50:22 MST 2013
Hi MC,

KEIL.

Thanks.
0 Kudos

411 Views
lpcware
NXP Employee
NXP Employee
Content originally posted in LPCWare by mc on Fri Dec 06 15:47:00 MST 2013
Hi Robert,
Which IDE are you using? Let me know I will post the code.

Thanks,
MC
0 Kudos