Hex file for IAP in lpc1788

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hex file for IAP in lpc1788

1,361件の閲覧回数
rameshlalji9595
Contributor II

Hello Everyone

I'm looking for how to read hex file from USB (USB Interfaced successfully) and decode the data in RAM for write into internal flash of lpc1788 for In-Application Programming. In which format data should be read and write into flash ? If anyone has sample code that would be grateful. 

Thanks in advance.

ラベル(1)
3 返答(返信)

1,275件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  Ramesh Lalji ,

You can google HEX file format, know meaning of each part, then you will know which part should write into flash.

 GENERAL: INTEL HEX FILE FORMAT 

And it seems you are working on a second bootloader, there are some application, you can refer to:

https://www.nxp.com/docs/en/application-note/AN10866.zip  

https://www.nxp.com/docs/en/application-note/AN11628.zip  

Regards,

Alice

1,275件の閲覧回数
rameshlalji9595
Contributor II

Hello Alice_Yang 
Thanks for sharing information. Its really helpful for me. 
But I'm actually working on code (Not like bootloader) that update firmware from USB when needed. 
And I wrote hex file to flash but I couldn't jump to my loaded code. Ir repeat code that existing in it.

Does Hex file starting address should be same as flash starting address? 

Thanks in advance 

0 件の賞賛

1,275件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Ramesh,

There is address information in Hex file,for example the below hex file, the highlight part is address.

pastedImage_1.png

You should refer to your hex file to flash.

BTW, you use USB update firmware, which memory you put the USB related code ?

Regards

Alice

0 件の賞賛