I am using LPC-link 2 2ith NHS3152TEMOADK: NHS3152 General Starter Kit, with LPCXpresso IDE.
When debugging blinky example, or any other example, i get:
LPCXpresso RedlinkMulti Driver v8.2 (Sep 5 2016 10:12:38 - crt_emu_cm_redlink build 725)
Found chip XML file in C:/Users/leo/Documents/LPCXpresso_8.2.2_650/workspace/app_example_blinky/Debug/Generic-M0plus.xml
Probe Firmware: LPC-LINK2 CMSIS-DAP V5.173 (NXP Semiconductors)
Serial Number: I3FUNVCT
VID:PID: 1FC9:0090
USB Path: \\?\hid#vid_1fc9&pid_0090&mi_00#7&2bf3e870&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
Cannot halt processor
Cannot halt processor
Emu(0): Connected&Reset. DpID: 0BC11477. CpuID: 410CC600. Info: <None>
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
Cannot halt processor
Failed on chip setup: Ep(04). Cannot halt processor.
How do I solve this? how do i reset it so that it works again ?
已解决! 转到解答。
Hi,
The example application app_example_dp_ndeft2t doesn't use Power-off or Deep Power Down modes, so once it is running, the debug interface should be readily available too.
With a battery inserted, without an NFC field, measuring 90mv between VDD and P11 indicates a problem with your battery connection..
With a plenished battery inserted, you should be able to measure ~3.4V between VDD and GND contact points.
Without a battery, when an NFC field is present, the whole IC will be powered by the NFC field, giving ~1.8V, as you also have measured.
It is good to read it's working now. I would definitely check on your battery, and play with the blinky demo app_demo_dp_blinky to learn the easiest - least painful - way to reliably connect and debug using this board.
Good luck!
Best,
Dries.
Hi Dries,
The chip is running again now, i have attached answeres to the questions anyhow cause maybe you can point me to the issue.
Since it is working again and nhs31xx/example.ndef is on it without reflashing it. I gather this was always on it.
The LPC-Link2 board already came with a jumper over JP2. I haven't removed them.
The following are Scope results:
NO NFC field: VDD and P11 have 90mv
WITH NFC: P7, P0,P9 1.8 V
NO NFC; LPC-link powered via USB: VDD 3.3V, P10 3.3, P11 3V
NFC and LPC-link powered via USB: i must have reset it whilst doing this, because all of a sudden it started to take me to nxp.com/etc..
after this it starting to run nhs31xx/example.ndef
I do, it's working.
What is the reset procedure i accidentaly found that i could reuse in the future?
Best,
Leo
Hi,
The example application app_example_dp_ndeft2t doesn't use Power-off or Deep Power Down modes, so once it is running, the debug interface should be readily available too.
With a battery inserted, without an NFC field, measuring 90mv between VDD and P11 indicates a problem with your battery connection..
With a plenished battery inserted, you should be able to measure ~3.4V between VDD and GND contact points.
Without a battery, when an NFC field is present, the whole IC will be powered by the NFC field, giving ~1.8V, as you also have measured.
It is good to read it's working now. I would definitely check on your battery, and play with the blinky demo app_demo_dp_blinky to learn the easiest - least painful - way to reliably connect and debug using this board.
Good luck!
Best,
Dries.
Hello Leo,
Your problem does not look obvious, let me probe a bit:
Kind regards,
Dries.
not sure if this is useful, but after i run the flash i get this from RedlinkServer
[Started server]
[Connected on port 3025]
redlink>ProbeList
Index = 1
Manufacturer = NXP Semiconductors
Description = LPC-LINK2 CMSIS-DAP V5.173
Serial Number = I3FUNVCT
VID:PID = 1FC9:0090
Path = \\?\hid#vid_1fc9&pid_0090&mi_00#7&2bf3e870&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
redlink>ProbeStatus
Index = 1
Manufacturer = NXP Semiconductors
Description = LPC-LINK2 CMSIS-DAP V5.173
Serial Number = I3FUNVCT
VID:PID = 1FC9:0090
Path = \\?\hid#vid_1fc9&pid_0090&mi_00#7&2bf3e870&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
IsOpen = FALSE
WireInitialized = FALSE
WireProtocol = JTAG
CoresConfigured = FALSE
PacketSize = 1024
Reference Count = 0
HasSWV = FALSE
HasETM = FALSE
HasJTAG = TRUE
HasSWD = TRUE
Probe Type = CMSIS-DAP
Probe Reference Count = 0
redlink>ProbeStatus
Index = 1
Manufacturer = NXP Semiconductors
Description = LPC-LINK2 CMSIS-DAP V5.173
Serial Number = I3FUNVCT
VID:PID = 1FC9:0090
Path = \\?\hid#vid_1fc9&pid_0090&mi_00#7&2bf3e870&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
IsOpen = FALSE
WireInitialized = FALSE
WireProtocol = JTAG
CoresConfigured = FALSE
PacketSize = 1024
Reference Count = 0
HasSWV = FALSE
HasETM = FALSE
HasJTAG = TRUE
HasSWD = TRUE
Probe Type = CMSIS-DAP
Probe Reference Count = 0
redlink>quit
[Closed]
Hi Xiangjun,
What do you mean ?
the LPC-link2 led comes on and flashes, But i cannot upload code without getting the Cannot halt processor message.
Is the issue with the code i am uploading ? Because i have tried to upload several different examples.
Best,
Leo
I tried using the ISP reset over debug, and got:
Ni: LPCXpresso RedlinkMulti Driver v8.2 (Sep 5 2016 10:12:38 - crt_emu_cm_redlink.exe build 725)
Pc: ( 0) Reading remote configuration
Nc: Found chip XML file in C:/Users/leo/Documents/LPCXpresso_8.2.2_650/workspace/app_example_dp_i2c/Debug_SLAVE/Generic-M0plus.xml
Pc: ( 5) Remote configuration complete
Wc: ============= SCRIPT: ISPResetConnect.scp =============
Wc: Reset to ISP
Wc: ============= END SCRIPT ==============================
Xe:
Nc: Probe Firmware: LPC-LINK2 CMSIS-DAP V5.173 (NXP Semiconductors)
Nc: Serial Number: I3FUNVCT
Nc: VID:PID: 1FC9:0090
Nc: USB Path: \\?\hid#vid_1fc9&pid_0090&mi_00#7&2bf3e870&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
Pc: ( 30) Emulator Connected
Xw:
Wc: Cannot halt processor
Wc: Cannot halt processor
Pc: ( 40) No Halt
Pc: ( 50) CPU ID
Nc: Emu(0): Connected&Reset. DpID: 0BC11477. CpuID: 410CC600. Info: <None>
Nc: Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
Wc: Cannot halt processor
Ed:03: Failed on chip setup: Ep(04). Cannot halt processor.
Pc: ( 65) Chip Setup Complete