Active faults while debugging on MCU Xpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Active faults while debugging on MCU Xpresso

898 Views
tanmayparashar9
Contributor I

Hello,

I am trying to run a LED AWS example on the LPC 54018 module. When I finish building the program and I debug it I am facing an issue which corresponds to something like active faults. Hence I am not able to see the output on Tera Term.

Please may I know where the issue is?

I have attached a screenshot of the active faults and my program folder below.

Thank You

Regards,

Tanmay

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

815 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Tanmay Parashar,

Please download the latest SDK version of SDK_2.5.0 to test the AWS demo under it.

https://mcuxpresso.nxp.com/en/builder   

Also refer to the readme.txt under SDK demo to configure and prepare the project.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply