AN12278 Section 2.3.2.1 - How to trigger SPI Flash SB2.1 firmware load from application

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AN12278 Section 2.3.2.1 - How to trigger SPI Flash SB2.1 firmware load from application

452 次查看
awseiger
Contributor I

The title says it all - In AN12278, Section 2.3.2.1, the following blurb exists:

"Staging media model. During OTA, a firmware update capsule in SB2.1 file format can be downloaded to the external SPI flash. Once the image is downloaded and validated, the running firmware can invoke a SPI recovery boot using the ROM API. On re-boot the ROM will execute the newly loaded SB2.1 file to update the main flash."

Where can I find documentation/examples for how to accomplish this?

0 项奖励
1 回复

422 次查看
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @awseiger,

Additional information can be found in the RM, section 6.4.3. (Link).

Best Regards,

Alexis Andalon

0 项奖励