关于pins-tool-for-imx-processors-v5-1_amd64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

关于pins-tool-for-imx-processors-v5-1_amd64

493 Views
alj79
Contributor II

我用pins-tool-for-imx-processors-v5-1_amd64生成的设备树文件片段如下:

/dts-v1/;

#include "skeleton.dtsi"
#include "imx6ull-pinfunc.h"

...............................................

&iomuxc {
    pinctrl-names = "default";
    pinctrl-0 = <&BOARD_InitPins>;
    imx6ull-board {
        BOARD_InitPins: BOARD_InitPinsGrp {                /*!< Function assigned for the core: Cortex-A7[ca7] */
            fsl,pins = <
                MX6ULL_PAD_ENET2_RX_ER__ECSPI4_SS0         0x000010B0
                MX6ULL_PAD_ENET2_TX_CLK__ECSPI4_MISO       0x000010B0
                MX6ULL_PAD_ENET2_TX_DATA1__ECSPI4_SCLK     0x000010B0
                MX6ULL_PAD_ENET2_TX_EN__ECSPI4_MOSI        0x000010B0
            >;
        };
    };
};

.......................................................

但是在linux下的imx6ull-pinfunc.h中没有MX6ULL_PAD_ENET2_RX_ER__ECSPI4_SS0,MX6ULL_PAD_ENET2_TX_CLK__ECSPI4_MISO,MX6ULL_PAD_ENET2_TX_DATA1__ECSPI4_SCLK和MX6ULL_PAD_ENET2_TX_EN__ECSPI4_MOSI的定义。

请问怎么能够将pins-tool-for-imx-processors-v5-1_amd64工具生成的设备树文件能够用在linux下?

我用的是linux4.1.15

0 Kudos
1 Reply

391 Views
jimmychan
NXP TechSupport
NXP TechSupport

For your reference, it is the same issue on Pins tool generate invalid imx6ull-board.dtsi .

Basically, the pins tool output is for reference. The i.MX6ULL is using the same pinfunc.h file of i.MX6UL. The pad name can be found in the i.MX6ul pinfunc.h file (imx6ul-pinfunc.h) So, you can just change the prefix of each PAD name from MX6ULL to MX6UL then it should work.

0 Kudos