关于GD25Q64芯片的参考代码

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

关于GD25Q64芯片的参考代码

1,767 次查看
sjrenyj
Contributor I

你好!

      请问有SPI方式的Nor Flash 型号为GD25Q64的参考代码吗?我看网上似乎是有相关才考代码的,但是没有找到。方便提供一下吗?

标签 (2)
0 项奖励
10 回复数

1,409 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi 娟 陈 ,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.
Before answering your question, whether you can tell me what chip you use now.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

1,409 次查看
sjrenyj
Contributor I

Hi,

I use LPC11U68 chip.  Thanks

0 项奖励

1,409 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi 娟 陈,

Thanks for your reply.
After a round of searching, I find that there's no similar demo code as you requested, so I'd highly recommend you to refer to the periph_ssp demo in the LPCOpen library whose download is below.

LPCOpen Software for LPC11XX|NXP
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

1,409 次查看
sjrenyj
Contributor I

你好,

我主要需要于GD25Q64相关芯片的.c和.h文件。我搜索柜论坛,似乎贵公司有开发板是用过GD25Q80芯片。

麻烦,再找找!多谢

在 2018-12-17 10:50:01,"jeremyzhou" <admin@community.nxp.com> 写道:

|

|

NXP Community

|

|

Re: 关于GD25Q64芯片的参考代码

reply from jeremyzhou in LPC Microcontrollers - View the full discussion

Hi 娟 陈,

Thanks for your reply.

After a round of searching, I find that there's no similar demo code as you requested, so I'd highly recommend you to refer to the periph_ssp demo in the LPCOpen library whose download is below.

LPCOpen Software for LPC11XX|NXP

Have a great day,

TIC

0 项奖励

1,409 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi 娟 陈

Thanks for your reply.

请告知你的说的板子名称,方便查找。
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

1,409 次查看
sjrenyj
Contributor I

如果告到那么详细,我自己都已经下载了。好不

0 项奖励

1,409 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi 娟 陈

告知更多的信息就是为了查找,因为之前我查过了,没有找到。

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励

1,409 次查看
sjrenyj
Contributor I

我服了。

在 2018-12-18 10:56:11,"jeremyzhou" <admin@community.nxp.com> 写道:

|

|

NXP Community

|

|

Re: 关于GD25Q64芯片的参考代码

reply from jeremyzhou in LPC Microcontrollers - View the full discussion

Hi 娟 陈,

Thanks for your reply.

请告知你的说的板子名称,方便查找。

Have a great day,

TIC

0 项奖励

1,409 次查看
sjrenyj
Contributor I

Hi,

     I use LPC11U68 chip. Looking forward to your replay!

    Thanks!

0 项奖励

1,409 次查看
sjrenyj
Contributor I

Hi,

I use LPC11U68 chip. Looking forward to your reply!

在 2018-12-14 10:07:55,"jeremyzhou" <admin@community.nxp.com> 写道:

|

|

NXP Community

|

|

Re: 关于GD25Q64芯片的参考代码

reply from jeremyzhou in LPC Microcontrollers - View the full discussion

Hi 娟 陈 ,

Thank you for your interest in NXP Semiconductor products and the opportunity to serve you.

Before answering your question, whether you can tell me what chip you use now.

Have a great day,

TIC

0 项奖励