emWin支持哪些编译器/IDE?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

emWin支持哪些编译器/IDE?

4,093件の閲覧回数
lpcware-support
Senior Contributor I

恩智浦在LPCware.com上有ARM/Keil, IAR, Rowley Crossworks和LPCXpresso的安装包。如有需要,以后会添加对其他编译器的支持。

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

3,433件の閲覧回数
Lambert
NXP Employee
NXP Employee

HI Lpcware_Support,

My csutomer is using I.MX7D(CotexA7+M4) on their project, and they are running FreeRTOS on M4. they are planning to  port emWin on FreeRTOS running with M4,  and they are using

/******************************************************************/

GCC revision 4.9-2015-q1-update from ARM Embedded

******************************************************************/

cross-compiler to compile FreeRTOS, is it possible to provide emWin lib which generated by GCC revision 4.9-2015-q1-update from ARM Embedded to customer?  Pls comment.

 

 

Thanks,

Lambert

0 件の賞賛
返信