emWin支持哪些编译器/IDE?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

emWin支持哪些编译器/IDE?

4,065 次查看
lpcware-support
Senior Contributor I

恩智浦在LPCware.com上有ARM/Keil, IAR, Rowley Crossworks和LPCXpresso的安装包。如有需要,以后会添加对其他编译器的支持。

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

3,405 次查看
Lambert
NXP Employee
NXP Employee

HI Lpcware_Support,

My csutomer is using I.MX7D(CotexA7+M4) on their project, and they are running FreeRTOS on M4. they are planning to  port emWin on FreeRTOS running with M4,  and they are using

/******************************************************************/

GCC revision 4.9-2015-q1-update from ARM Embedded

******************************************************************/

cross-compiler to compile FreeRTOS, is it possible to provide emWin lib which generated by GCC revision 4.9-2015-q1-update from ARM Embedded to customer?  Pls comment.

 

 

Thanks,

Lambert

0 项奖励
回复