adc dma pdb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

adc dma pdb

1,742件の閲覧回数
benelghali
Contributor II

hello everybody,

I'm using KV31F256 microcontroller and KSDK 1.2 on IAR Embedded workbench.

Here is my problem i configured dma channel 0 on pdb request and in this transfer i configured ADC0 SC1A register throw a buffer i created so  it can generate a soft trigger to begin adc0 conversion.

In the other hand i configured dma channel 1 on ADC0 COCO request to transfer data from ADC0 RA to a buffer i created.

So regarding to this configuration i expected to have one conversion after each PDB request.

To check this i configured a dma channel1 interrupt and i set then reset a pin to see a pulse at the oscilloscope each time a conversion is complete.

here is my problem i got a continuous train of pulses that are not synchronized with the pdb request so i checked the adc0 and it is not configured in continuous mode so i didn't understand why i didn't have the desired behavior.

Can anyone help me please.

Thanks.

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 返信

1,521件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I am curious if you have clear the DMA CH1 related interrupt request and Done Flag.

Wish it helps.


Have a great day,
Ma Hui

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信