I am using KDS sample project dspi_blocking_example_master_frdmk22f provided with Kinetis SDK 1.2.0 to initiate SPI transfer from FRDM K22F board. The sample project should configure the microcontroller as master and configure SPI0 interface.
If I connect an oscilloscope to pins PTC4 (PCS0), PTC5 (SCK), PTC6 (MISO), PTC7 (MOSI), I don't see any output from these pins. I also tried using AARDVARK SPI adapter and I am unable to receive any data on that either.
Since it's a sample project, I thought it should just work fine. Can you please suggest me if I am doing anything wrong?
Hello Richard,
Do you have two FRDM-K22 board ? If you have , please connect the two board to test.
I have test the DSPI demo of KSDK1.2, it can work well , i refer to the DOC of "Kinetis SDK v.1.2.0 Demo Applications User's Guide.pdf" (under here :\Freescale\KSDK_1.2.0\doc) to connect the pins :
then i can see the result at putty :
So the demo code with no error. The reason why you not the the spi signal is the MASTER only send
once for the project , so the oscilloscope can not catch it or we can not see it . You can try to change the
code to make MASTER board send data for while , then it can see in the oscilloscope.
Hope it helps
Alice
Hello Priya,
Have you refer to the DOC of Kinetis SDK v.1.2.0 Demo Applications User's Guide.pdf here : \Freescale\KSDK_1.2.0\doc ?
I have test the project on FRDM-K64 board , it can work well , be sure the pins have been connect correctly .
And also does the characters can printed through UART correctly ?
BR
Alice